SectionLineStyleBuilderCreateSectionLineType Enumeration¶
NXOpen.Drawings.SectionLineStyleBuilder.CreateSectionLineType is an alias for NXOpen.Drawings.SectionLineStyleBuilderCreateSectionLineType
-
class
NXOpen.Drawings.
SectionLineStyleBuilderCreateSectionLineType
¶ Bases:
object
This enum represents whether or not to create a view for the section line.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.ShowSectionLineType
instead.Enum Members
Enum Member Enum Member Description WithView WithoutView -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-