DraftingViewCollection Class¶
-
class
NXOpen.Drawings.
DraftingViewCollection
¶ Bases:
object
Represents a collection of :py:class:`NXOpen.Drawings.DraftingView`s.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
ConvertLegacyViewsToLightweight | Converts legacy views to lightweight. |
CreateAddRemoveBoxViewBuilder | Creates a NXOpen.Drawings.AddRemoveBoxViewBuilder @return |
CreateBaseViewBuilder | Creates the Base View Builder @return |
CreateBrokenViewBuilder | Creates a NXOpen.Drawings.BrokenViewBuilder @return |
CreateCopyTo3dBuilder | Creates a NXOpen.Drawings.ViewCopyTo3dBuilder @return |
CreateCustomViewSettingsBuilder | Creates a NXOpen.Drawings.CustomViewSettingsBuilder @return |
CreateDetailViewBuilder | Creates a NXOpen.Drawings.DetailViewBuilder @return |
CreateDrawingViewBuilder | Creates a DrawingViewBuilder @return |
CreateProjectedViewBuilder | Creates the Projected View Builder @return |
CreateRefineDisplayBuilder | Creates a NXOpen.Drawings.RefineDisplayBuilder @return |
CreateSectionInViewBuilder | Creates the Section In View Builder @return |
CreateSectionViewBuilder | Creates the Section View Builder @return |
CreateShipDraftingViewLinesBuilder | Creates a NXOpen.Drawings.ShipDraftingViewLinesBuilder @return Returns the empty Ship Drafting View Lines sub-builder on View Style |
CreateShipbuildingLineBuilder | Creates a NXOpen.Drawings.ViewStyleShipbuildingLinesBuilder @return Returns the empty Shipbuilding Lines sub-builder on View Style |
CreateStandardViewsBuilder | Creates a StandardViewsBuilder @return |
CreateUpdateViewsBuilder | Creates the Update Views Builder @return |
CreateViewCreationWizardBuilder | Creates a NXOpen.Drawings.ViewCreationWizardBuilder @return |
CreateViewProjectionBuilder | Creates a NXOpen.Drawings.ViewProjectionBuilder @return |
DeleteViewsInOriginalPart | Deletes views in original part |
FindObject | Finds the NXOpen.Drawings.DraftingView with the given identifier as recorded in a journal. |
GetParentOfView | Find the parent cut (sectioned) model view of a drawing member view. |
MoveViewsToDrawing | Move views to drawing |
PasteViews | Paste views |
RestoreViewBreaks | Restore all view breaks of the view suppressed by Drawings.DraftingViewCollection.SuppressViewBreaks |
SuppressViewBreaks | Suppress all view breaks of the view. |
UpdateViewBreaks | Log all view breaks of the view for update |
UpdateViews | Updates drafting views in the part determined by an update option. |
Enumerations¶
DraftingViewCollectionViewCopyAnnotOption Enumeration | Specifies the the annotation copy mode. |
DraftingViewCollectionViewCopyDetailOption Enumeration | Specifies the the view copy mode. |
DraftingViewCollectionViewUpdateOption Enumeration | Specifies which drafting views to update. |
Method Detail¶
ConvertLegacyViewsToLightweight¶
-
DraftingViewCollection.
ConvertLegacyViewsToLightweight
¶ Converts legacy views to lightweight.
The views in list can be spread amongst multiple sheets, but they must all belong to the same part.
Signature
ConvertLegacyViewsToLightweight(views)
Parameters: views (list of NXOpen.Drawings.DraftingView
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
CreateAddRemoveBoxViewBuilder¶
-
DraftingViewCollection.
CreateAddRemoveBoxViewBuilder
¶ Creates a
NXOpen.Drawings.AddRemoveBoxViewBuilder
Signature
CreateAddRemoveBoxViewBuilder(activeView)
Parameters: activeView – the active view. Cannot be None. :type activeView:
NXOpen.Drawings.DraftingView
:returns: :rtype:NXOpen.Drawings.AddRemoveBoxViewBuilder
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
CreateBaseViewBuilder¶
-
DraftingViewCollection.
CreateBaseViewBuilder
¶ Creates the Base View Builder
Signature
CreateBaseViewBuilder(view)
Parameters: view ( NXOpen.Drawings.BaseView
) – the base view to be edited, if None, then create a base viewReturns: Return type: NXOpen.Drawings.BaseViewBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateBrokenViewBuilder¶
-
DraftingViewCollection.
CreateBrokenViewBuilder
¶ Creates a
NXOpen.Drawings.BrokenViewBuilder
Signature
CreateBrokenViewBuilder(viewbreak)
Parameters: viewbreak ( NXOpen.Drawings.ViewBreak
) – the view break to be edited, None in case of new broken view.Returns: Return type: NXOpen.Drawings.BrokenViewBuilder
New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
CreateCopyTo3dBuilder¶
-
DraftingViewCollection.
CreateCopyTo3dBuilder
¶ Creates a
NXOpen.Drawings.ViewCopyTo3dBuilder
Signature
CreateCopyTo3dBuilder()
Returns: Return type: NXOpen.Drawings.ViewCopyTo3dBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateCustomViewSettingsBuilder¶
-
DraftingViewCollection.
CreateCustomViewSettingsBuilder
¶ Creates a
NXOpen.Drawings.CustomViewSettingsBuilder
Signature
CreateCustomViewSettingsBuilder()
Returns: Return type: NXOpen.Drawings.CustomViewSettingsBuilder
New in version NX8.5.0.
License requirements: drafting (“DRAFTING”)
CreateDetailViewBuilder¶
-
DraftingViewCollection.
CreateDetailViewBuilder
¶ Creates a
NXOpen.Drawings.DetailViewBuilder
Signature
CreateDetailViewBuilder(view)
Parameters: view ( NXOpen.Drawings.DetailView
) –NXOpen.Drawings.DetailView
to be edited, if None then create a new oneReturns: Return type: NXOpen.Drawings.DetailViewBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateDrawingViewBuilder¶
-
DraftingViewCollection.
CreateDrawingViewBuilder
¶ Creates a DrawingViewBuilder
Signature
CreateDrawingViewBuilder(drawingview)
Parameters: drawingview ( NXOpen.Drawings.DrawingView
) – the drawing view to be edited, if None, then create a drawing viewReturns: Return type: NXOpen.Drawings.DrawingViewBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateProjectedViewBuilder¶
-
DraftingViewCollection.
CreateProjectedViewBuilder
¶ Creates the Projected View Builder
Signature
CreateProjectedViewBuilder(view)
Parameters: view ( NXOpen.Drawings.ProjectedView
) – the projected view to be edited, if None, then create a projected viewReturns: Return type: NXOpen.Drawings.ProjectedViewBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateRefineDisplayBuilder¶
-
DraftingViewCollection.
CreateRefineDisplayBuilder
¶ Creates a
NXOpen.Drawings.RefineDisplayBuilder
Signature
CreateRefineDisplayBuilder()
Returns: Return type: NXOpen.Drawings.RefineDisplayBuilder
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
CreateSectionInViewBuilder¶
-
DraftingViewCollection.
CreateSectionInViewBuilder
¶ Creates the Section In View Builder
Signature
CreateSectionInViewBuilder()
Returns: Return type: NXOpen.Drawings.SectionInViewBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateSectionViewBuilder¶
-
DraftingViewCollection.
CreateSectionViewBuilder
¶ Creates the Section View Builder
Signature
CreateSectionViewBuilder(sectionViewOrSectionLine)
Parameters: sectionViewOrSectionLine ( NXOpen.NXObject
) – the section view or section line to be edited, if None, then create a section view or section lineReturns: Return type: NXOpen.Drawings.SectionViewBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreateShipDraftingViewLinesBuilder¶
-
DraftingViewCollection.
CreateShipDraftingViewLinesBuilder
¶ Creates a
NXOpen.Drawings.ShipDraftingViewLinesBuilder
Signature
CreateShipDraftingViewLinesBuilder()
Returns: Returns the empty Ship Drafting View Lines sub-builder on View Style Return type: NXOpen.Drawings.ShipDraftingViewLinesBuilder
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
CreateShipbuildingLineBuilder¶
-
DraftingViewCollection.
CreateShipbuildingLineBuilder
¶ Creates a
NXOpen.Drawings.ViewStyleShipbuildingLinesBuilder
Signature
CreateShipbuildingLineBuilder()
Returns: Returns the empty Shipbuilding Lines sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleShipbuildingLinesBuilder
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
CreateStandardViewsBuilder¶
-
DraftingViewCollection.
CreateStandardViewsBuilder
¶ Creates a StandardViewsBuilder
Signature
CreateStandardViewsBuilder()
Returns: Return type: NXOpen.Drawings.StandardViewsBuilder
New in version NX6.0.1.
License requirements: nx_layout (“NX Layout”)
CreateUpdateViewsBuilder¶
-
DraftingViewCollection.
CreateUpdateViewsBuilder
¶ Creates the Update Views Builder
Signature
CreateUpdateViewsBuilder()
Returns: Return type: NXOpen.Drawings.UpdateViewsBuilder
New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
CreateViewCreationWizardBuilder¶
-
DraftingViewCollection.
CreateViewCreationWizardBuilder
¶ Creates a
NXOpen.Drawings.ViewCreationWizardBuilder
Signature
CreateViewCreationWizardBuilder()
Returns: Return type: NXOpen.Drawings.ViewCreationWizardBuilder
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
CreateViewProjectionBuilder¶
-
DraftingViewCollection.
CreateViewProjectionBuilder
¶ Creates a
NXOpen.Drawings.ViewProjectionBuilder
Signature
CreateViewProjectionBuilder()
Returns: Return type: NXOpen.Drawings.ViewProjectionBuilder
New in version NX6.0.2.
License requirements: nx_layout (“NX Layout”)
DeleteViewsInOriginalPart¶
-
DraftingViewCollection.
DeleteViewsInOriginalPart
¶ Deletes views in original part
Signature
DeleteViewsInOriginalPart(views)
Parameters: views (list of NXOpen.Drawings.DraftingView
) –New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
FindObject¶
-
DraftingViewCollection.
FindObject
¶ Finds the
NXOpen.Drawings.DraftingView
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the drafting view to be found Returns: View with this identifier Return type: NXOpen.Drawings.DraftingView
New in version NX3.0.0.
License requirements: None.
GetParentOfView¶
-
DraftingViewCollection.
GetParentOfView
¶ Find the parent cut (sectioned) model view of a drawing member view.
If the parent view is not a cut model view, None is returned.
Signature
GetParentOfView(view)
Parameters: view ( NXOpen.View
) –Returns: Return type: NXOpen.ModelingView
New in version NX3.0.0.
License requirements: None.
MoveViewsToDrawing¶
-
DraftingViewCollection.
MoveViewsToDrawing
¶ Move views to drawing
Signature
MoveViewsToDrawing(views, drawing)
Parameters: - views (list of
NXOpen.Drawings.DraftingView
) – new views - drawing (
NXOpen.Drawings.DrawingSheet
) – the drawing which view will in
New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
- views (list of
PasteViews¶
-
DraftingViewCollection.
PasteViews
¶ Paste views
Signature
PasteViews(drawing, views, detailOption, annotOption)
Parameters: - drawing (
NXOpen.Drawings.DrawingSheet
) – the drawing which view in - views (list of
NXOpen.Drawings.DraftingView
) – old views - detailOption (
NXOpen.Drawings.DraftingViewCollectionViewCopyDetailOption
) – detail copy option - annotOption (
NXOpen.Drawings.DraftingViewCollectionViewCopyAnnotOption
) – Annotation copy option
Returns: new views
Return type: list of
NXOpen.Drawings.DraftingView
New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
- drawing (
RestoreViewBreaks¶
-
DraftingViewCollection.
RestoreViewBreaks
¶ Restore all view breaks of the view suppressed by
Drawings.DraftingViewCollection.SuppressViewBreaks
Signature
RestoreViewBreaks(view)
Parameters: view ( NXOpen.Drawings.DraftingView
) –New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
SuppressViewBreaks¶
-
DraftingViewCollection.
SuppressViewBreaks
¶ Suppress all view breaks of the view.
It is neccessary if we want change the view contents
Signature
SuppressViewBreaks(view)
Parameters: view ( NXOpen.Drawings.DraftingView
) –New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
UpdateViewBreaks¶
-
DraftingViewCollection.
UpdateViewBreaks
¶ Log all view breaks of the view for update
Signature
UpdateViewBreaks(view)
Parameters: view ( NXOpen.Drawings.DraftingView
) – View in which view breaks will be updatedNew in version NX8.5.0.
License requirements: drafting (“DRAFTING”)
UpdateViews¶
-
DraftingViewCollection.
UpdateViews
¶ Overloaded method UpdateViews
UpdateViews(updateOption)
UpdateViews(updateOption, drawing)
UpdateViews(views)
-------------------------------------
Updates drafting views in the part determined by an update option. For example, to update all out of date views in a part, pass in
Drawings.DraftingViewCollectionViewUpdateOption.OutOfDate
.Signature
UpdateViews(updateOption)
Parameters: updateOption ( NXOpen.Drawings.DraftingViewCollectionViewUpdateOption
) – View update optionNew in version NX3.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Updates drafting views in a sheet determined by an update option. For example, to update all out of date views on the sheet, pass in
Drawings.DraftingViewCollectionViewUpdateOption.OutOfDate
.Signature
UpdateViews(updateOption, drawing)
Parameters: - updateOption (
NXOpen.Drawings.DraftingViewCollectionViewUpdateOption
) – View update option - drawing (
NXOpen.Drawings.DrawingSheet
) –
New in version NX3.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Updates the drafting views. The views in list can be spread amongst multiple sheets, but they must all belong to the same part.
Signature
UpdateViews(views)
Parameters: views (list of NXOpen.Drawings.DraftingView
) –New in version NX3.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------