ShipDraftingViewLinesBuilder Class¶
-
class
NXOpen.Drawings.
ShipDraftingViewLinesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a ship view lines block
To create a new instance of this class, use
NXOpen.Drawings.DraftingViewCollection.CreateShipDraftingViewLinesBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
NonSectionedHiddenColor | Returns or sets the non-sectioned hidden color on the Ship Structure Lines |
NonSectionedHiddenFont | Returns or sets the non-sectioned hidden font on the Ship Structure Lines |
NonSectionedHiddenWidth | Returns or sets the non-sectioned hidden width on the Ship Structure Lines |
NonSectionedVisibleColor | Returns or sets the non-sectioned visible color on the Ship Structure Lines |
NonSectionedVisibleFont | Returns or sets the non-sectioned visible font on the Ship Structure Lines |
NonSectionedVisibleWidth | Returns or sets the non-sectioned visible width on the Ship Structure Lines |
SectionedHiddenColor | Returns or sets the sectioned hidden color on the Ship Structure Lines |
SectionedHiddenFont | Returns or sets the sectioned hidden font on the Ship Structure Lines |
SectionedHiddenWidth | Returns or sets the sectioned hidden width on the Ship Structure Lines |
SectionedVisibleColor | Returns or sets the sectioned visible color on the Ship Structure Lines |
SectionedVisibleFont | Returns or sets the sectioned visible font on the Ship Structure Lines |
SectionedVisibleWidth | Returns or sets the sectioned visible width on the Ship Structure Lines |
SingleLineRepresentation | Returns or sets the single line representation toggle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NonSectionedVisibleColor¶
-
ShipDraftingViewLinesBuilder.
NonSectionedVisibleColor
¶ Returns or sets the non-sectioned visible color on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedVisibleColor()
Returns: Returns the non-sectioned visible color that is on the ship drafting view lines sub-builder Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedVisibleColor(nonSectionedVisibleColor)
Parameters: nonSectionedVisibleColor (Id) – Sets a new non-sectined visible color on the ship drafting view lines sub-builder New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedVisibleFont¶
-
ShipDraftingViewLinesBuilder.
NonSectionedVisibleFont
¶ Returns or sets the non-sectioned visible font on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedVisibleFont()
Returns: Returns the non-sectioneed visible font that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedVisibleFont(nonSectionedVisibleFont)
Parameters: nonSectionedVisibleFont ( NXOpen.Preferences.Font
) – Sets a new non-sectioned visible font on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedVisibleWidth¶
-
ShipDraftingViewLinesBuilder.
NonSectionedVisibleWidth
¶ Returns or sets the non-sectioned visible width on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedVisibleWidth()
Returns: Returns the non-sectioned visible width that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedVisibleWidth(nonSectionedVisibleWidth)
Parameters: nonSectionedVisibleWidth ( NXOpen.Preferences.Width
) – Sets a new non-sectioned visible width on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedVisibleColor¶
-
ShipDraftingViewLinesBuilder.
SectionedVisibleColor
¶ Returns or sets the sectioned visible color on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedVisibleColor()
Returns: Returns the sectioned visible color that is on the ship drafting view lines sub-builder Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedVisibleColor(sectionedVisibleColor)
Parameters: sectionedVisibleColor (Id) – Sets a new sectined visible color on the ship drafting view lines sub-builder New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedVisibleFont¶
-
ShipDraftingViewLinesBuilder.
SectionedVisibleFont
¶ Returns or sets the sectioned visible font on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedVisibleFont()
Returns: Returns the sectioneed visible font that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedVisibleFont(sectionedVisibleFont)
Parameters: sectionedVisibleFont ( NXOpen.Preferences.Font
) – Sets a new sectioned visible font on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedVisibleWidth¶
-
ShipDraftingViewLinesBuilder.
SectionedVisibleWidth
¶ Returns or sets the sectioned visible width on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedVisibleWidth()
Returns: Returns the sectioned visible width that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedVisibleWidth(sectionedVisibleWidth)
Parameters: sectionedVisibleWidth ( NXOpen.Preferences.Width
) – Sets a new sectioned visible width on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SingleLineRepresentation¶
-
ShipDraftingViewLinesBuilder.
SingleLineRepresentation
¶ Returns or sets the single line representation toggle
-------------------------------------
Getter Method
Signature
SingleLineRepresentation()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleLineRepresentation(singleLineRepresentation)
Parameters: singleLineRepresentation (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Method Detail¶
Validate¶
-
ShipDraftingViewLinesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.