InspectionSetup Class¶
-
class
NXOpen.CAM.
InspectionSetup
¶ Bases:
NXOpen.CAM.CAMObject
Inspection setup
Use the
Part
class to get or create an inspection setupNew in version NX7.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BufferObjects | Buffer objects to the clipboard and prepare for copy later |
CopyObjects | Copy objects @return array of new objects |
CreateNcmctPartMountingBuilder | Creates a Part Mounting Builder. |
CreateObjectsUdeSet | Create ObjectsUdeSet. |
CutObjects | Cut objects |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GenerateToolPath | Generate tool path |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetBooleanValue | Get the boolean value of the parameter index from the object @return the boolean value |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFeedRate | Get the feed rate value and unit of the parameter index from the object @return the feed rate unit |
GetFeedRateColor | Get the feed rate color of the parameter index from the object. |
GetIntegerArrayValue | Get the integer array value of the parameter index from the object. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetIntegerValue | Get the integer value of the parameter index from the object. |
GetObject | Get the object value of the parameter index from the object @return the object value |
GetObjectArrayValue | Get the object array value of the parameter index from the object. |
GetRealArrayValue | Get the real array value of the parameter index from the object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetRealValue | Get the real value of the parameter index from the object. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRoot | Get root of the specified branch. |
GetStatus | Get the status of the input object. |
GetStringArrayValue | Get the string array value of the parameter index from the object. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetStringValue | Get the string value of the parameter index from the object @return the string value |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetWireEdmFeedRate | Get the feed rate value and side of the parameter index from the object, side is only used in wire edm. |
Has911Attribute | Check if a 911 attribute exists in an object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
LockToolPaths | Lock Tool Path |
MoveObjects | Move objects |
PasteObjects | Paste objects after cut |
Postprocess | Postprocess |
PostprocessWithSetting | Postprocess |
Prints a representation of this object to the system log file. | |
Remove911Attribute | Remove a specific 911 attribute from an object. |
RemoveAll911Attributes | Remove all 911 attributes from an object. |
ResequencePaths | Resequence selected paths using nearest neighbor order |
ResequenceTols | Resequence tolerances |
RetrieveDevice | Retrieve a device from library @return machine device created |
RetrievePathMessages | Retrieve toolpath validation messages @return array of message strings |
RetrieveTool | Retrieve a tool from library @return created the tool library |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetBooleanValue | Set a boolean value to the parameter index for the object. |
SetFeedRate | Set feed rate value and unit to the parameter index for the object. |
SetFeedRateColor | Set feed rate display color to the parameter index for the object. |
SetIntegerArrayValue | Set integer array value to the parameter index for the object. |
SetIntegerValue | Set an integer value to the parameter index for the object. |
SetName | Sets the custom name of the object. |
SetObject | Set a object to the parameter index for the object. |
SetObjectArrayValue | Set object array to the parameter index for the object |
SetRealArrayValue | Set real array to the parameter index for the object. |
SetRealValue | Set a real value to the parameter index for the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetStringArrayValue | Set string array to the parameter index for the object |
SetStringValue | Set a string value to the parameter index for the object. |
SetTemplateStatus | Set Template status |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetWireEdmFeedRate | Set feed rate value and side to the parameter index for the object, side is only used in wire edm. |
UpdateFeatureNames | Update feature names in referencing operations. |
Property Detail¶
IsOccurrence¶
-
InspectionSetup.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
InspectionSetup.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
InspectionSetup.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
InspectionSetup.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
InspectionSetup.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
InspectionSetup.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
BufferObjects¶
-
InspectionSetup.
BufferObjects
¶ Buffer objects to the clipboard and prepare for copy later
Signature
BufferObjects(view, objectsToBeBuffered)
Parameters: - view (
NXOpen.CAM.CAMSetupView
) – view - objectsToBeBuffered (list of
NXOpen.CAM.CAMObject
) – array of objects to be buffered
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- view (
CopyObjects¶
-
InspectionSetup.
CopyObjects
¶ Copy objects
Signature
CopyObjects(view, objectsToBeMoved, destinationObject, pastePosition)
Parameters: - view (
NXOpen.CAM.CAMSetupView
) – view - objectsToBeMoved (list of
NXOpen.CAM.CAMObject
) – array of objects to be moved - destinationObject (
NXOpen.CAM.CAMObject
) – the destination object - pastePosition (
NXOpen.CAM.CAMSetupPaste
) – paste inside or after the destination object
Returns: array of new objects
Return type: list of
NXOpen.CAM.CAMObject
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- view (
CreateNcmctPartMountingBuilder¶
-
InspectionSetup.
CreateNcmctPartMountingBuilder
¶ Creates a Part Mounting Builder.
Note: Commit a Part Mounting Builder will perform the Part Mounting and no object is returned.
Signature
CreateNcmctPartMountingBuilder(libRef)
Parameters: libRef (str) – a unique library reference identifier NOTE: The full Unicode character set is not supported for this parameter. Returns: part mounting builder created Return type: NXOpen.CAM.NcmctPartMountingBuilder
New in version NX8.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CreateObjectsUdeSet¶
-
InspectionSetup.
CreateObjectsUdeSet
¶ Create ObjectsUdeSet.
Signature
CreateObjectsUdeSet(params, udeType)
Parameters: - params (list of
NXOpen.CAM.CAMObject
) – array of operations or groups - udeType (
NXOpen.CAM.CAMSetupUde
) – ude type
Returns: created objects ude set
Return type: New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- params (list of
CutObjects¶
-
InspectionSetup.
CutObjects
¶ Cut objects
Signature
CutObjects(view, objectsToBeMoved)
Parameters: - view (
NXOpen.CAM.CAMSetupView
) – view - objectsToBeMoved (list of
NXOpen.CAM.CAMObject
) – array of objects to be moved
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- view (
FindObject¶
-
InspectionSetup.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GenerateToolPath¶
-
InspectionSetup.
GenerateToolPath
¶ Generate tool path
Signature
GenerateToolPath(objects)
Parameters: objects (list of NXOpen.CAM.CAMObject
) – array of objectsNew in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GetRoot¶
-
InspectionSetup.
GetRoot
¶ Get root of the specified branch.
Signature
GetRoot(branch)
Parameters: branch ( NXOpen.CAM.CAMSetupView
) – Branch from which to get setup rootReturns: Root of the specified branch Return type: NXOpen.CAM.InspectionGroup
New in version NX9.0.3.
License requirements: None.
LockToolPaths¶
-
InspectionSetup.
LockToolPaths
¶ Lock Tool Path
Signature
LockToolPaths(objects, lock)
Parameters: - objects (list of
NXOpen.CAM.CAMObject
) – array of objects - lock (bool) – lock the tool path if true, else unlock the tool path
New in version NX7.5.4.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- objects (list of
MoveObjects¶
-
InspectionSetup.
MoveObjects
¶ Move objects
Signature
MoveObjects(view, objectsToBeMoved, destinationObject, pastePosition)
Parameters: - view (
NXOpen.CAM.CAMSetupView
) – view - objectsToBeMoved (list of
NXOpen.CAM.CAMObject
) – array of objects to be moved - destinationObject (
NXOpen.CAM.CAMObject
) – the destination object - pastePosition (
NXOpen.CAM.CAMSetupPaste
) – paste inside or after the destination object
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- view (
PasteObjects¶
-
InspectionSetup.
PasteObjects
¶ Paste objects after cut
Signature
PasteObjects(view, objectsToBeMoved, destinationObject, pastePosition)
Parameters: - view (
NXOpen.CAM.CAMSetupView
) – view - objectsToBeMoved (list of
NXOpen.CAM.CAMObject
) – array of objects to be pasted - destinationObject (
NXOpen.CAM.CAMObject
) – the destination object - pastePosition (
NXOpen.CAM.CAMSetupPaste
) – paste inside or after the destination object
New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- view (
Postprocess¶
-
InspectionSetup.
Postprocess
¶ Signature
Postprocess(objects, machineType, outfileName, outputUnits)
Parameters: - objects (list of
NXOpen.CAM.CAMObject
) – array of objects - machineType (str) – machine type NOTE: The full Unicode character set is not supported for this parameter.
- outfileName (str) – output file name NOTE: The full Unicode character set is not supported for this parameter.
- outputUnits (
NXOpen.CAM.CAMSetupOutputUnits
) – output file unit
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- objects (list of
PostprocessWithSetting¶
-
InspectionSetup.
PostprocessWithSetting
¶ Postprocess
Signature
PostprocessWithSetting(objects, machineType, outfileName, outputUnits, outputWarning, reviewTool)
Parameters: - objects (list of
NXOpen.CAM.CAMObject
) – array of objects - machineType (str) – machine type NOTE: The full Unicode character set is not supported for this parameter.
- outfileName (str) – output file name NOTE: The full Unicode character set is not supported for this parameter.
- outputUnits (
NXOpen.CAM.CAMSetupOutputUnits
) – output file unit - outputWarning (
NXOpen.CAM.CAMSetupPostprocessSettingsOutputWarning
) – whether ouput warning file - reviewTool (
NXOpen.CAM.CAMSetupPostprocessSettingsReviewTool
) – whether active review tool window
New in version NX8.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- objects (list of
Print¶
-
InspectionSetup.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ResequencePaths¶
-
InspectionSetup.
ResequencePaths
¶ Resequence selected paths using nearest neighbor order
Signature
ResequencePaths(paths)
Parameters: paths (list of NXOpen.CAM.CAMObject
) – array of paths to resequenceNew in version NX9.0.0.
License requirements: None.
ResequenceTols¶
-
InspectionSetup.
ResequenceTols
¶ Resequence tolerances
Signature
ResequenceTols(tols)
Parameters: tols (list of NXOpen.CAM.CAMObject
) – array of tolerances to resequenceNew in version NX9.0.0.
License requirements: None.
RetrieveDevice¶
-
InspectionSetup.
RetrieveDevice
¶ Retrieve a device from library
Signature
RetrieveDevice(libRef)
Parameters: libRef (str) – a unique library reference identifier NOTE: The full Unicode character set is not supported for this parameter. Returns: machine device created Return type: NXOpen.CAM.InspectionGroup
New in version NX8.0.0.
License requirements: None.
RetrievePathMessages¶
-
InspectionSetup.
RetrievePathMessages
¶ Retrieve toolpath validation messages
Signature
RetrievePathMessages(objects)
Parameters: objects (list of NXOpen.CAM.CAMObject
) – array of object tagsReturns: array of message strings Return type: list of str New in version NX9.0.0.
License requirements: None.
RetrieveTool¶
-
InspectionSetup.
RetrieveTool
¶ Overloaded method RetrieveTool
RetrieveTool(libRef)
RetrieveTool(libRef, target)
-------------------------------------
Retrieve a tool from library
Signature
RetrieveTool(libRef)
Parameters: libRef (str) – the library name NOTE: The full Unicode character set is not supported for this parameter. Returns: a tuple Return type: A tuple consisting of (libTool, success). libTool is a NXOpen.CAM.InspectionTool
. created the tool library success is a bool.New in version NX7.5.1.
License requirements: None.
-------------------------------------
Retrieve a tool from library to the target
Signature
RetrieveTool(libRef, target)
Parameters: - libRef (str) – the library name NOTE: The full Unicode character set is not supported for this parameter.
- target (
NXOpen.CAM.CAMObject
) – the target where the tool is mounted
Returns: a tuple
Return type: A tuple consisting of (libTool, nextTarget, success). libTool is a
NXOpen.CAM.InspectionTool
. created the tool library nextTarget is aNXOpen.CAM.CAMObject
. the next target where the tool can be mounted success is a bool.New in version NX8.5.0.
License requirements: None.
-------------------------------------
SetName¶
-
InspectionSetup.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetTemplateStatus¶
-
InspectionSetup.
SetTemplateStatus
¶ Set Template status
Signature
SetTemplateStatus(objects, useAsParent, createIfParentCreated)
Parameters: - objects (list of
NXOpen.CAM.CAMObject
) – array of objects to adjust - useAsParent (bool) – object can be used as a template or not
- createIfParentCreated (bool) – create if parent is created
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- objects (list of
UpdateFeatureNames¶
-
InspectionSetup.
UpdateFeatureNames
¶ Update feature names in referencing operations.
Signature
UpdateFeatureNames(originalFeatName, newFeatName)
Parameters: - originalFeatName (str) – Original feature name NOTE: The full Unicode character set is not supported for this parameter.
- newFeatName (str) – New feature name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.3.
License requirements: None.