CAMSetupPostprocessSettingsOutputWarning Enumeration

NXOpen.CAM.CAMSetup.PostprocessSettingsOutputWarning is an alias for NXOpen.CAM.CAMSetupPostprocessSettingsOutputWarning

class NXOpen.CAM.CAMSetupPostprocessSettingsOutputWarning

Bases: object

Output warning setting for Postprocess

Enum Members

Enum Member Enum Member Description
Yes
output the warning file
No
not output the warning file
PostDefined
use post defined setting
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.