CAMSetupPostprocessSettingsReviewTool Enumeration

NXOpen.CAM.CAMSetup.PostprocessSettingsReviewTool is an alias for NXOpen.CAM.CAMSetupPostprocessSettingsReviewTool

class NXOpen.CAM.CAMSetupPostprocessSettingsReviewTool

Bases: object

Review tool setting for Postprocess

Enum Members

Enum Member Enum Member Description
On
show the review tool window
Off
not show the review tool window
PostDefined
use post defined setting
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.