CAMSetupOutputUnits Enumeration¶
NXOpen.CAM.CAMSetup.OutputUnits is an alias for NXOpen.CAM.CAMSetupOutputUnits
-
class
NXOpen.CAM.
CAMSetupOutputUnits
¶ Bases:
object
Output units used in output clsf and postprocess.
Enum Members
Enum Member Enum Member Description Inch use inch as output unitMetric use metric as output unitPostDefined use post defined unit as output unit-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-