BodyCollection Class¶
-
class
NXOpen.
BodyCollection
¶ Bases:
object
Represents a collection of bodies in a part
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateFourPointSurfaceBuilder | Creates a Four Point Surface Builder @return FourPointSurfaceBuilder object |
CreateSurfaceUvdirectionBuilder | Creates a SurfaceUVDirectionBuilder @return |
FindObject | Finds the NXOpen.Body with the given identifier as recorded in a journal. |
Method Detail¶
CreateFourPointSurfaceBuilder¶
-
BodyCollection.
CreateFourPointSurfaceBuilder
¶ Creates a Four Point Surface Builder
Signature
CreateFourPointSurfaceBuilder()
Returns: FourPointSurfaceBuilder object Return type: NXOpen.FourPointSurfaceBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
CreateSurfaceUvdirectionBuilder¶
-
BodyCollection.
CreateSurfaceUvdirectionBuilder
¶ Creates a SurfaceUVDirectionBuilder
Signature
CreateSurfaceUvdirectionBuilder()
Returns: Return type: NXOpen.SurfaceUVDirectionBuilder
New in version NX8.5.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FindObject¶
-
BodyCollection.
FindObject
¶ Finds the
NXOpen.Body
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the body you want Returns: Body with this identifier Return type: NXOpen.Body
New in version NX3.0.0.
License requirements: None.