FourPointSurfaceBuilder Class¶
-
class
NXOpen.
FourPointSurfaceBuilder
¶ Bases:
NXOpen.Builder
Represents a four point sheet body builder
To create a new instance of this class, use
NXOpen.BodyCollection.CreateFourPointSurfaceBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Point1 | Returns or sets the first point |
Point2 | Returns or sets the second point |
Point3 | Returns or sets the third point |
Point4 | Returns or sets the fourth point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Point1¶
-
FourPointSurfaceBuilder.
Point1
¶ Returns or sets the first point
-------------------------------------
Getter Method
Signature
Point1()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point1(point1)
Parameters: point1 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Point2¶
-
FourPointSurfaceBuilder.
Point2
¶ Returns or sets the second point
-------------------------------------
Getter Method
Signature
Point2()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point2(point2)
Parameters: point2 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Point3¶
-
FourPointSurfaceBuilder.
Point3
¶ Returns or sets the third point
-------------------------------------
Getter Method
Signature
Point3()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point3(point3)
Parameters: point3 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Point4¶
-
FourPointSurfaceBuilder.
Point4
¶ Returns or sets the fourth point
-------------------------------------
Getter Method
Signature
Point4()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point4(point4)
Parameters: point4 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
Validate¶
-
FourPointSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.