CenterlineCollection Class¶
-
class
NXOpen.Annotations.
CenterlineCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.Centerline
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateAutomaticCenterlineBuilder | Creates the AutomaticCenterlineBuilder @return AutomaticCenterlineBuilder object |
CreateBoltCircleCenterlineBuilder | Creates the BoltCircleCenterline builder @return BoltCircleCenterlineBuilder object |
CreateCenterMarkBuilder | Creates the CenterMark Builder @return CenterMarkBuilder Object |
CreateCenterline2dBuilder | Creates the 2D Centerline builder @return Centerline2dBuilder object |
CreateCenterline3dBuilder | Creates the 3D Centerline builder @return Annotations. |
CreateCircularCenterlineBuilder | Creates the CircularCenterline builder @return CircularCenterlineBuilder object |
CreatePmiCenterMarkBuilder | Creates the Pmi CenterMark Builder @return PmiCenterMarkBuilder Object |
CreatePmiCenterline3dBuilder | Creates the Pmi 3D Centerline builder @return PmiCenterline3dBuilder object |
CreateSymmetricalCenterlineBuilder | Creates the Symmetrical Centerline builder @return SymmetricalCenterlineBuilder object |
FindObject | Finds the Centerline with the given name. |
Method Detail¶
CreateAutomaticCenterlineBuilder¶
-
CenterlineCollection.
CreateAutomaticCenterlineBuilder
¶ Creates the AutomaticCenterlineBuilder
Signature
CreateAutomaticCenterlineBuilder()
Returns: AutomaticCenterlineBuilder object Return type: NXOpen.Annotations.AutomaticCenterlineBuilder
New in version NX6.0.0.
License requirements: None.
CreateBoltCircleCenterlineBuilder¶
-
CenterlineCollection.
CreateBoltCircleCenterlineBuilder
¶ Creates the BoltCircleCenterline builder
Signature
CreateBoltCircleCenterlineBuilder(centerline)
Parameters: centerline ( NXOpen.Annotations.BoltCircleCenterline
) –NXOpen.Annotations.BoltCircleCenterline
to be edited, if None then create a new oneReturns: BoltCircleCenterlineBuilder object Return type: NXOpen.Annotations.BoltCircleCenterlineBuilder
New in version NX6.0.0.
License requirements: None.
CreateCenterMarkBuilder¶
-
CenterlineCollection.
CreateCenterMarkBuilder
¶ Creates the CenterMark Builder
Signature
CreateCenterMarkBuilder(centerline)
Parameters: centerline ( NXOpen.Annotations.CenterMark
) –NXOpen.Annotations.CenterMark
to be edited, if None then create a new oneReturns: CenterMarkBuilder Object Return type: NXOpen.Annotations.CenterMarkBuilder
New in version NX6.0.0.
License requirements: None.
CreateCenterline2dBuilder¶
-
CenterlineCollection.
CreateCenterline2dBuilder
¶ Creates the 2D Centerline builder
Signature
CreateCenterline2dBuilder(cline)
Parameters: cline ( NXOpen.Annotations.Centerline2d
) –NXOpen.Annotations.Centerline2d
to be editedReturns: Centerline2dBuilder object Return type: NXOpen.Annotations.Centerline2dBuilder
New in version NX6.0.0.
License requirements: None.
CreateCenterline3dBuilder¶
-
CenterlineCollection.
CreateCenterline3dBuilder
¶ Creates the 3D Centerline builder
Signature
CreateCenterline3dBuilder(cline)
Parameters: cline ( NXOpen.Annotations.Centerline3d
) –NXOpen.Annotations.Centerline3d
to be editedReturns: Annotations.Centerline3dBuilder object Return type: NXOpen.Annotations.Centerline3dBuilder
New in version NX6.0.0.
License requirements: None.
CreateCircularCenterlineBuilder¶
-
CenterlineCollection.
CreateCircularCenterlineBuilder
¶ Creates the CircularCenterline builder
Signature
CreateCircularCenterlineBuilder(centerline)
Parameters: centerline ( NXOpen.Annotations.CircularCenterline
) –NXOpen.Annotations.CircularCenterline
to be edited, if None then create a new oneReturns: CircularCenterlineBuilder object Return type: NXOpen.Annotations.CircularCenterlineBuilder
New in version NX6.0.0.
License requirements: None.
CreatePmiCenterMarkBuilder¶
-
CenterlineCollection.
CreatePmiCenterMarkBuilder
¶ Creates the Pmi CenterMark Builder
Signature
CreatePmiCenterMarkBuilder(centerline)
Parameters: centerline ( NXOpen.Annotations.PmiCenterMark
) –NXOpen.Annotations.PmiCenterMark
to be edited, if None then create a new oneReturns: PmiCenterMarkBuilder Object Return type: NXOpen.Annotations.PmiCenterMarkBuilder
New in version NX7.5.0.
License requirements: None.
CreatePmiCenterline3dBuilder¶
-
CenterlineCollection.
CreatePmiCenterline3dBuilder
¶ Creates the Pmi 3D Centerline builder
Signature
CreatePmiCenterline3dBuilder(cline)
Parameters: cline ( NXOpen.Annotations.PmiCenterline3d
) –NXOpen.Annotations.PmiCenterline3d
to be editedReturns: PmiCenterline3dBuilder object Return type: NXOpen.Annotations.PmiCenterline3dBuilder
New in version NX7.5.0.
License requirements: None.
CreateSymmetricalCenterlineBuilder¶
-
CenterlineCollection.
CreateSymmetricalCenterlineBuilder
¶ Creates the Symmetrical Centerline builder
Signature
CreateSymmetricalCenterlineBuilder(centerline)
Parameters: centerline ( NXOpen.Annotations.SymmetricalCenterline
) –NXOpen.Annotations.SymmetricalCenterline
to be edited, if None then create a new oneReturns: SymmetricalCenterlineBuilder object Return type: NXOpen.Annotations.SymmetricalCenterlineBuilder
New in version NX6.0.0.
License requirements: None.
FindObject¶
-
CenterlineCollection.
FindObject
¶ Finds the Centerline with the given name.
An exception will be thrown if no object can be found with given name
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the centerline to be found Returns: Centerline with this identifier Return type: NXOpen.Annotations.Centerline
New in version NX6.0.0.
License requirements: None.