SymmetricalCenterlineBuilder Class¶
-
class
NXOpen.Annotations.
SymmetricalCenterlineBuilder
¶ Bases:
NXOpen.Annotations.CenterlineBuilder
Builder for creating Symmetrical Centerline.
It creates or edits Symmetrical Centerline To create a new instance of this class, use
NXOpen.Annotations.CenterlineCollection.CreateSymmetricalCenterlineBuilder
Default values.
Property Value Settings.Extension 6.35 (millimeters part), 0.25 (inches part) Settings.Gap 1.5875 (millimeters part), 0.0625 (inches part) Settings.IndividualDistance 0 Settings.Size 3.175 (millimeters part), 0.125 (inches part) Settings.Width Thin Type FromFace New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
End | Returns the end object of Symmetrical Centerline |
Face | Returns the face object of Symmetrical Centerline |
Inherit | Returns the inherit object |
Settings | Returns the settings builder object for Symmetrical Centerline |
Start | Returns the start object of Symmetrical Centerline |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of Symmetrical Centerline |
Methods¶
Method | Description |
---|---|
AddEndExtensions | Adds extensions only at ends |
AddExtension | Adds extension based on select object index |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllExtensions | Returns all extensions. |
GetAllIndividualExtensions | Returns individual extensions. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEndExtensions | Returns end extensions only. |
GetObject | Returns the object currently being edited by this builder. |
RemoveEndExtensions | Removes extensions only at ends |
RemoveExtension | Removes extension based on select object index |
ResetAllExtensions | Reset all extensions by the supplied defaultValue |
SetAllIndividualExtensions | Sets all individual extensions |
SetEndExtensions | Modifies end extensions only |
SetIndividualExtensions | Modifies extensions based on select object index |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SymmetricalCenterlineBuilderTypes Enumeration | the valid types of Symmetrical Centerline |
Property Detail¶
End¶
-
SymmetricalCenterlineBuilder.
End
¶ Returns the end object of Symmetrical Centerline
-------------------------------------
Getter Method
Signature
End()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Face¶
-
SymmetricalCenterlineBuilder.
Face
¶ Returns the face object of Symmetrical Centerline
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Inherit¶
-
SymmetricalCenterlineBuilder.
Inherit
¶ Returns the inherit object
-------------------------------------
Getter Method
Signature
Inherit()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Settings¶
-
SymmetricalCenterlineBuilder.
Settings
¶ Returns the settings builder object for Symmetrical Centerline
-------------------------------------
Getter Method
Signature
Settings()
Returns: Return type: NXOpen.Annotations.SymmetricalCenterlineSettingsBuilder
New in version NX6.0.0.
License requirements: None.
Start¶
-
SymmetricalCenterlineBuilder.
Start
¶ Returns the start object of Symmetrical Centerline
-------------------------------------
Getter Method
Signature
Start()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Type¶
-
SymmetricalCenterlineBuilder.
Type
¶ Returns or sets the type of Symmetrical Centerline
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Annotations.SymmetricalCenterlineBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Annotations.SymmetricalCenterlineBuilderTypes
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
SymmetricalCenterlineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.