BoltCircleCenterlineBuilder Class¶
-
class
NXOpen.Annotations.
BoltCircleCenterlineBuilder
¶ Bases:
NXOpen.Annotations.CircleCenterlineBuilder
Represents a BoltCircleCenterlineBuilder Builder
To create a new instance of this class, use
NXOpen.Annotations.CenterlineCollection.CreateBoltCircleCenterlineBuilder
Default values.
Property Value FullCircle true Type Through3Points New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
FullCircle | Returns or sets the method which returns full or partial circle flag |
Inherit | Returns the inherit object |
Locations | Returns the selction object of the centerline |
Settings | Returns the settings builder object for the centerline |
Tag | Returns the Tag for this object. |
Type | Returns or sets the method which returns type of centerline |
Methods¶
Method | Description |
---|---|
AddEndExtensions | Adds extensions only at ends |
AddExtension | Adds extension based on select object index |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllExtensions | Returns all extensions. |
GetAllIndividualExtensions | Returns individual extensions. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEndExtensions | Returns end extensions only. |
GetObject | Returns the object currently being edited by this builder. |
RemoveEndExtensions | Removes extensions only at ends |
RemoveExtension | Removes extension based on select object index |
RemoveLocation | Removes location object for a given index from the Select Object List. |
ResetAllExtensions | Reset all extensions by the supplied defaultValue |
SetAllIndividualExtensions | Sets all individual extensions |
SetEndExtensions | Modifies end extensions only |
SetIndividualExtensions | Modifies extensions based on select object index |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
BoltCircleCenterlineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.