Document sidebar selector
The Document sidebar selector is available when editing a Document. It can display any of several sidebars showing Comments, Document Outline, and other information about the current Document. There is also access to tools such as Test Run Planning. Select the desired sidebar via the sidebar drop-down menu on the Document Editor toolbar.
Commands |
---|
Note:
Some sidebars are not available when viewing a Document in read-only mode.
(Due to permissions, or because you're viewing a baseline or revision.)