Test Run Planning sidebar
Usage: Populate a Test Run with Test Cases from the current Document.
Document filtered for relevant Test Cases. | Add to Waiting. |
Remove from Waiting. | Remove selected from Waiting. (If already in queue.) |
Add selected items to Waiting. | Multiple items selected. |
This panel enables you to select Test Cases to be tested when a Test Run is performed by testers.
Component descriptions:
Displays the ID of the Test Run for which Test Cases are being selected or removed. (Read only)
Displays the name of the template on which the Test Run shown in ID is based. (Read only)
Shows a count of the Test Cases currently populating the Test Run.
Shows a count of the Test Cases current populating the Test Run which have not currently been tested.
Adds one or more Test Cases, selected in the Document body, to the queue of waiting Test Cases for the Test Run. Enabled when the Test Case(s) not already in the Waiting queue is/are selected in the Document.
Removes one or more selected Test Cases, selected in the Document body, from the queue of waiting Test Cases for the Test Run. Enabled when the Test Case(s) already in the Waiting queue is/are selected in the Document.
Displays the total estimated time needed to test all Test Cases currently populating the Test Run. Each Test Case has a field for storing the estimated time needed to test it.
Saves the current Test Case selection to the Test Run.