Information for authors and managers
This section contains information for authors and/or managers of specification or other Documents. It covers what you need to know in order to set up a review and sign-off process for your Documents.
Start by working with the Polarion administrator for your project to review the Document Types and Document Workflow configurations to make sure the types you need exist, and that each type has your process mapped in the workflow. Decide which transition actions must require signatures, and have each action configured accordingly in the Document workflow configuration. Information for administrators is provided in Configure Document Signatures. Depending on the project template used to create the project, very little if any modification may be needed.
With the Document signatures configuration in place, there is nothing more to do except develop your Document up to the point where it is ready for the workflow transition that requires signatures — or the first such, if there is more than one. For example, your Document starts with a Draft status, and at some point is ready for review and approval. Following the simple scenario described earlier, you would invoke the Send to Review action. The action is enabled in the Status field in the Document Properties because that action was not configured to require signatures in order for the transition to In Review status to take place.
However, you see that the next action, Mark Approved, is disabled in the Status field. This is because the action is configured to require signatures. You won't be able to invoke that action and transition the Document to the Approved status until signatures are logged. It is at this point that you need to invite people to review and sign your Document.
Invite people to review and sign
Everyone you invite must have a Polarion user account, and have permission to read Documents in the project. Otherwise, they cannot to see your Document and receive an error message if they follow a link leading to it. All reviewers must also be assigned the project role that has been granted the SIGN/DECLINE permission for Documents. Otherwise, they do not appear in the list of people you can invite to review and sign your Document.
User roles, and permissions granted to user roles, are determined by organization or project managers and configured by the Polarion administrator.
Open the Document in the Document Editor, and open the Signatures sidebar.
The sidebar shows a panel labeled with the name of the workflow action that requires signatures. In the case of our running example, that would be Mark Approved.
Click the action name. The sidebar shows two page tabs and a button.
Signature policy
Invite people to sign
Click Invite for Signature.
In the dialog, select the first user you want to invite from the user names in the drop-down list.
If you want to invite another user, click the icon, select the user in the list, and click again.
Repeat until you have added all the users you want to invite.
Tip:You cannot invoke the transition action until the configured signature policy is satisfied. For example, if the policy requires all invited users to sign, the action cannot be invoked until all have logged a signature. If it requires that at least one must sign and none must decline, then that condition must be satisfied in order to invoke the action.
You can view the signature policy in the All Signatures tab of the Signatures sidebar, shown after you click an action name. See the previous figure.
At the bottom of the dialog, select the URL in the Link for Invitees text box and copy it to your clipboard.
Click OK to close the dialog, and then click Save.
Open your email client program, or internet chat, etc. and compose a message to all the people you invited, asking them to review and sign the document. Paste the URL from your clipboard into the message body.
Add users. |
Users added. |
Copy URL for email. |
The following figure illustrates an email message to invite people to review and sign a Document.
When sending a message to your reviewers, include the Document URL. Paste the Document URL from the Invite for Signature dialog box.
Automate the invitees List
Your administrator can predefine the list of invitees for any Document workflow action, so that the Document owner/manager does not have to add invitees manually for every new Document. Invitees can be added according to their user role in the project, or explicitly by their user ID. You might want to consider having custom user roles defined for your project and have those roles assigned to the people who routinely review and approve specifications or other kinds of Documents.
Monitor signatures
You can monitor the progress of collecting signatures in the Signatures sidebar of your Document. The sidebar shows which invitees have signed, which have declined, and the names of all invitees.
The All Signatures tab of the sidebar shows this same information, plus the signature policy.
If the signature policy is currently satisfied, a message displays indicating this. A link is provided that opens the Document Properties sidebar. You can then invoke the action to transition the Document in the Status field, where the action is enabled. Be sure to save the Document after changing the field.
Restart the process
Sometimes feedback from invited signers reveals that additional work on the Document is necessary. In that case, another round of reviews needs to be started. The Document owner/manager can reset signature status of Signed or Rejected for the current workflow transition back to the Pending state by clicking on the X icon on the right part of the signature Statistics. The Reset action is available only in the All Signatures panel for a specific workflow transition — the is, not in My Signatures, and not in Entry Point). It is not available after the Document status has been transitioned. You can see recalculated signature statistics immediately without saving the Document.
In cases where a Document needs to be reworked, or a signature was declined, the author or owner may decide that signatures up to that point are obsolete and a new round of reviews and signatures is needed on a new, reworked Document version. To accommodate such scenarios, an administrator can configure the workflow action that sends the Document back to the authoring status — Back to Draft) to run a workflow function that marks the current signatures as obsolete.
Complete the process
After all signatures needed to satisfy the signature policy have been logged, the Signatures sidebar displays a message indicating that the Document can now be transitioned to the next Status. You as the Document owner, author or manager must explicitly take this action.
Transition the signed Document:
Open the Document Properties sidebar.
Click the drop-down control of the Status field.
Select the signed workflow action in the list. The list item should now be enabled.
Save the Document.
To be able to transition the workflow, you must have the MANAGE SIGNATURES permission for Documents, assuming your system has the default configuration of workflow signatures.
As you can see in the above figure, when signature policy is satisfied, the workflow transition action is enabled.
Pending signatures | Signatures done |
Action disabled | Action enabled |
When the signature policy is satisfied, the All Signatures tab of the Signatures sidebar displays a link that, when clicked, opens the Document Properties sidebar, where you can change the Document Status.
In projects based on Polarion Project Templates, requirements specification type Documents are preconfigured with Document workflow and permissions settings that make such Documents read-only once they have reached any other than the Draft status in the workflow. The prevents modification of any Requirements Specification Document that was submitted for review or approved. Documents can be branched to store the approved version of Document for implementation, while the master specification can be worked on for a subsequent version or release. For technical details, see Document Signatures Custom Set.