Teamcenter must be restarted after modifying preferences.
View these preferences in
an .xls
file.
The dataset type defined in all auxiliary_types preferences (CATIA_xxx_auxiliary_types) is case-sensitive and must match with the case used in Teamcenter's BMIDE.
Define the list of analysis auxiliary file types. There is no default value for this setting.
Multiple values are permitted.
CATIA_analysis_auxiliary_types
Define the dataset type used by the Integration to manage CATAnalysis auxiliary files by setting CATIA_analysis_xxx_aux_dataset_type, where xxx = auxiliary file type defined in CATIA_analysis_auxiliary_types.
CATIA_analysis_xxx_aux_dataset_type = CATxxx
There is no default value.
Link type between a CATAnalysis dataset and an auxiliary dataset, where xxx = auxiliary file type defined in CATIA_analysis_auxiliary_types.
CATIA_analysis_xxx_aux_link_on_dataset = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Link type between an item revision and an auxiliary dataset of a CATAnalysis file, where xxx = auxiliary file type defined in CATIA_analysis_auxiliary_types.
CATIA_analysis_xxx_aux_link_on_item_rev = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Define the list of drawing auxiliary file types. There is no default value for this setting.
Multiple values are permitted.
CATIA_dwg_auxiliary_types
Define the dataset type used by the Integration to manage CATDrawing auxiliary files by setting CATIA_dwg_xxx_aux_dataset_type, where xxx = auxiliary file type defined in CATIA_dwg_auxiliary_types.
CATIA_dwg_xxx_aux_dataset_type = CATxxx
There is no default value.
Link type between a CATDrawing dataset and an Auxiliary dataset, where xxx = auxiliary file type defined in CATIA_dwg_auxiliary_types.
CATIA_dwg_xxx_aux_link_on_dataset = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Link type between an item revision and an auxiliary dataset of a CATDrawing file, where xxx = auxiliary file type defined in CATIA_analysis_auxiliary_types.
CATIA_dwg_xxx_aux_link_on_item_rev = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Define the list of part auxiliary file types. There is no default value for this setting.
Multiple values are permitted.
CATIA_part_auxiliary_types
Define the dataset type used by the Integration to manage CATPart auxiliary files by setting CATIA_part_xxx_aux_dataset_type, where xxx = auxiliary file type defined in CATIA_part_auxiliary_types.
CATIA_part_xxx_dataset_type = CATxxx
There is no default value.
Link type between a CATPart dataset and an auxiliary dataset, where xxx = auxiliary file type defined in CATIA_part_auxiliary_types.
CATIA_part_xxx_aux_link_on_dataset = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Link type between an item revision and an auxiliary dataset of a CATPart file, where xxx = auxiliary file type defined in CATIA_part_auxiliary_types.
CATIA_part_xxx_aux_link_on_item_rev = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Define the list of process auxiliary file types. There is no default value for this setting.
Multiple values are permitted.
CATIA_process_auxiliary_types
Define the dataset type used by the Integration to manage CATProcess auxiliary files by setting CATIA_process_xxx_aux_dataset_type, where xxx = auxiliary file type defined in CATIA_process_auxiliary_types.
CATIA_process_xxx_dataset_type = CATxxx
There is no default value.
Link type between a CATProcess dataset and an auxiliary dataset, where xxx = auxiliary file type defined in CATIA_process_auxiliary_types.
CATIA_process_xxx_aux_link_on_dataset = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Link type between an item revision and an auxiliary dataset of a CATProcess file, where xxx = auxiliary file type defined in CATIA_process_auxiliary_types.
CATIA_process_xxx_aux_link_on_item_rev = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Define the list of product auxiliary file types. There is no default value for this setting.
Multiple values are permitted.
CATIA_prod_auxiliary_types
Define the dataset type used by the Integration to manage CATProduct auxiliary files by setting CATIA_prod_xxx_aux_dataset_type, where xxx = auxiliary file type defined in CATIA_prod_auxiliary_types.
CATIA_prod_xxx_dataset_type = CATxxx
There is no default value.
Link type between a CATProduct dataset and an auxiliary dataset, where xxx = auxiliary file type defined in CATIA_prod_auxiliary_types.
CATIA_prod_xxx_aux_link_on_dataset = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Link type between an item revision and an auxiliary dataset of a CATProduct file, where xxx = auxiliary file type defined in CATIA_prod_auxiliary_types.
CATIA_prod_xxx_aux_link_on_item_rev = catia_auxiliaryLink
The default value is catia_auxiliaryLink.
Define the auxiliary file type for each CATIA primary type prior to saving auxiliary files. There is no default value for these settings.
Multiple values are permitted.
For example:
CATIA_part_auxiliary_types =
cgr
model
The link type must also be defined before linking the dataset to the item revision and the dataset to the CATIA primary type. The default value is catia_auxiliarylink.
For example:
CATIA_part_cgr_aux_link_on_item_rev = IMAN_Rendering
CATIA_part_cgr_aux_link_on_dataset = catia_CgmLink
Define the POM class used to create the user data on the link between a drawing dataset and an auxiliary dataset. This link is preserved during the post-action process and it is not case-sensitive.
CATIA_pom_class_auxiliary_link_userdata = newClassName
The default value is Cat2_POM_CatiaAuxiliaryLink.