If these variables are modified, restart Teamcenter to apply the new
values.
Name |
Default value |
Purpose |
TcIC_assyconfig_menu |
false |
Display Save Assembly Configuration command in the CATIA menu
in Teamcenter, in the contextual menu of a selected BOM Line in
the Teamcenter Loader and in the Load Manager (true).
Display the Activate Terminal Node command in the CATIA toolbar.
(true) |
TcIC_awhosted_menu |
false |
Display (true) or hide (false) the TcIC menu when Embedded
Active Workspace installation is defined. |
TcIC_catalog_dir |
%WORK_DIR%\catalog (WIN) |
Directory where Catalog files and related documents are stored |
TcIC_config_dir |
%USERPROFILE% (WIN) |
TcIC filepath for configuration files. |
TcIC_dr1_license |
false |
Support TcIC functionalities (true) when a DR1 license is used.
|
TcIC_export_dir |
%WORK_DIR%\Export (WIN)
|
Used only by CATIA
Export filepath |
TcIC_export_spreadsheet_path |
%WORK_DIR%\Export\ExpSpreadSheet.txt
(WIN) |
SpreadSheet file path for EXPORT process |
TcIC_files_dir |
%WORK_DIR%\catuii (WIN) |
Directory where product, part, drawing and model files are
stored |
TcIC_import_data_path |
%WORK_DIR%\Import\Data.txt (WIN) |
Used only by CATIA
Data filepath |
TcIC_import_dir |
%WORK_DIR%\Import (WIN) |
Used only by CATIA
Import filepath |
TcIC_import_spreadsheet_path |
%WORK_DIR%\Import\ImpSpreadSheet.txt
(WIN) |
Spreadsheet file path for IMPORT process |
TcIC_plmvis_license |
Base |
PLM Vis license used when displaying the Teamcenter Loader's
JT Viewer.
Possible values are Base, Standard, Pro and Mockup
NOTE: Teamcenter Integration for
CATIA officially only supports Base license. |
TcIC_rac_socket_port |
11401 |
TCP port number used for the interface communication between
RAC and RACLess. |
TcIC_socket_port |
11400 |
TCP port number for the interface communication and the progress
indicator. |
TcIC_tmp_dir |
%WORK_DIR%\tmp (WIN) |
Directory where temporary communication files are stored |
TcIC_web_server_port |
3000 |
TCP port number used for the Active Workspace web server |