Displays the File Open dialog box.
Visual Basic |
---|
Public Function GetOpenFileNameWithOptions( _ ByVal dwFlagForOpen As ULong, _ ByRef LinksUpdate As LinksUpdateOption, _ ByRef AltLinkPath As String, _ ByRef DocAccess As DocumentAccess, _ ByRef OptNotify As NotifyOption, _ ByRef DocRelationAutoServer As Object, _ Optional ByVal FileFilter As Variant, _ Optional ByVal FilterIndex As Variant, _ Optional ByVal Title As Variant, _ Optional ByVal IgnoreWarnings As Variant _ ) As Variant |
Value | Description |
---|---|
igLinksUpdateWithAltPath | Update links with alternate path |
igLinksUpdateWithDefpath | Update links with default path |
igNoLinksUpdate | Do not update links |
Value | Description |
---|---|
igReadExclusive | Document has exclusive read access |
igReadOnly | Document has read-only access |
igReadWrite | Document has read-write access |
Value | Description |
---|---|
igNoNotify | Do not notify |
igNotifyWhenAvailable | Notify when the document is available |
igNotifyWhenExclusive | Notify when the document is exclusive |
igNotifyWhenReadable | Notify when the document can be read |
igNotifyWhenWriteable | Notify when the document can be written |