AbortCommand | Aborts the active command. |
Activate | Makes the referenced object the active one. |
ArrangeWindows | Arranges windows |
BiDM_RegisterCustomProps | Register BiDM custom properties either from Propseed.txt or from Template file or from both |
ClearMRU | Resets the MRU list, backstage and any MRU controls on the ribbon/QAT. |
CommandEnabled | |
CreateCommand | Creates a Solid Edge command control. |
DisableBuilInDataMgmt | Disable BuiltIn Data Mgmt |
DisableEventsForGivenAddIn | Disable firing the events for this AddIn. |
DoIdle | Gives idle time to the application. Call the DoIdle() method to provide the application with the opportunity to perform background tasks that may not be up-to-date because of intense processing. |
EnableEventsForGivenAddIn | Enable firing the events for this AddIn. |
FindFile | Displays the Find File dialog box. |
FindSEDocumentsContainingText | Returns the list of Solid Edge files that contain given text. |
FindWhereUsedDocuments | Find where used for given files. |
GenerateMasterImportListForDataPrep | Generate Master import list for data preparation |
Get_Set_FileNamingRule | Get or set 'File Naming Rule' SE Option checkbox. True value means 'Use Document Number and Revision' rule set, False is for 'None'. |
Get_Set_UseBiDM_SEOption | Get or set 'Use Solid Edge Data Management' SE Option. True value means BiDM is ON, False is for ON. |
GetCountOfOpenModelsInFemap | Get count of models currently open in FEMAP |
GetDefaultTemplatePath | |
GetDirectoryName | Displays a directory browser dialog box and returns the selected directory name. |
GetDocNameFormulaForFile | Returns the Document name formula for the given file. |
GetDraftPrintUtility | An object that is used to print Draft files. |
GetGlobalParameter | Returns the setting of a specified global parameter for the referenced Application or document object. |
GetLatestRevision | Returns the latest revision far a given File. |
GetMaterialTable | |
GetNextDocumentNumbers | Returns the next Document Numbers generated from NumberGenerator.dat file. |
GetOpenFileName | Displays the File Open dialog box. |
GetOpenFileNameWithOptions | Displays the File Open dialog box. |
GetRevisionLinkInfo | Returns revision link information from file storage |
GetRevisionsHistory | Returns the Revisions History for a Solid Edge file. |
GetSaveAsFileName | Returns the new name of the file to save. |
GetSolidEdgeWorkflowInformation | Get Solid Edge Workflow used in SEDM for a file. |
GetTemplateFileName | This method gets the template file name specified by the document type. |
GetTopLevelAssemblyFileNames | |
MailLogoff | Closes an established MAPI mail session. |
MailLogon | Logs into MAPI mail and establishes a mail session. |
OpenDraft | Opens where-referenced draft documents for selected 3d documents. |
PerformSolidEdgeWorkflow | Perform workflow in SEDM. |
QuerySystemInformation | Query System Information |
Quit | Exits the referenced application. |
ReplaceReference | Determines the documents with a specified referenced in user-defined directories and replaces those references with the new reference. |
ResetConfigFile | |
ResumeMRU | Resumes adding files to the MRU during the current session. |
RunMacro | Executes a specified macro. |
SEAdminUpdate | |
SearchDocuments | Searched documents at specified managed/unmanaged location based of defined criteria |
SEGetFileVersionInfo | Returns the last saved and created version information of the file. |
SetAddInInterfaces | Preapre the map of AddIns and their corresponding interfaces |
SetBIDMATPInfo | |
SetBuiltInATPRunningFlagAndATPID | |
SetDefaultTemplatePath | |
SetGlobalParameter | Sets the value of a specified global parameter for the referenced Application or document object. |
SetMessageForBIDMCPD | |
SetOLERequestPendingTimeout | Determines in milliseconds the amount of time after an automation or OLE request is made before a busy message is displayed. The default value is 8000 milliseconds (8 seconds) |
SetOLEServerBusyTimeout | Determines in milliseconds how long Solid Edge will go on retrying your automation or OLE requests before displaying the Component Busy dialog. The default value is 10000 milliseconds (10 seconds). |
SetValuesForBIDMCPD | |
ShowCommand | |
StartCommand | Activates a specified Solid Edge command. |
SuspendMRU | Suspends adding files to the MRU duing the current session. |
WriteDocumentFormulaIntoXML |