Class Module | Description |
Accelerator | Represents a collection of KeyBinding objects. |
Accelerators | Represents a collection of Accelerator objects. |
AddIn | A control that represents a command added to Solid Edge through the AddIn interface. |
AddInEdgeBarEvents | |
AddInEvents | A collection of AddInEvent objects. |
AddIns | A collection of AddIn objects. |
AddInSaveAsTranslatorEvents | An interface that allows an add-in that has save as capability for Solid Edge files to respond to user interface events. |
AnimationEvents | Animation events. |
Application | Provides the properties and methods necessary for a Visual Basic user to drive Solid Edge programmatically. |
ApplicationEvents | Fires application events. |
ApplicationV8DocumentOpenEvent | Fires document open event |
ApplicationWindowEvents | Provides access to the application window events. |
AssemblyChangeEvents | Assembly change events. |
AssemblyConfigurationChangeEvents | Fires AssemblyConfigurationChange user interface events. |
AssemblyFamilyEvents | |
AssemblyFamilyEvents2 | |
AssemblyPhysicalPropertiesChangeEvents | Fires Assembly Physical Proeprties Change user interface events. |
AssemblyRecomputeEvents | Represents a collection of assembly recompute events. |
Attribute | Represents an occurrence of a user-defined attribute. |
AttributeQuery | Contains the QueryByName method, which enables you to locate attribute sets and individual attributes. |
AttributeSet | Represents an occurrence of a user-defined attribute set. |
AttributeSets | Represents a collection of AttributeSet objects. |
BeforeFileSaveAsEvents | Fires BeforeFileSaveAs user interface events. |
BendTableEvents | Fires Bend Table events. |
BiDMEvents | BiDM Events |
BlockTableEvents | Contains the AfterUpdate event. |
Command | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
CommandBar | Represents all menus, toolbars, and pop-up menus in Solid Edge. |
CommandBarButton | Represents buttons on toolbars and menus. |
CommandBarButtonEvents | A collection of CommandBarButtonEvent objects. |
CommandBarControl | Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects. |
CommandBarControls | Contains all of the buttons and pop-ups on a specific command bar. |
CommandBarPopup | Represents pop-ups on toolbars and menus. |
CommandBars | A collection of all of the command bars within a specific environment. |
CommandCategories | A collection of command categories |
CommandCategory | |
CommandInfo | |
CommandWindow | Triggers Command Window events. |
ConnectorTableEvents | Contains the AfterUpdate event. |
CPDInitializer | |
CPDInitializerBiDM | |
CPDInitializerInsightXT | |
Customization | An object that is sued to Customize the UI |
DashStyle | The DashStyle object represents a custom dash style in a Draft document. |
DashStyles | The DashStyles object represents a collection of DashStyle objects. |
DISEAddInEvents | A collection of AddInEvent objects. |
DISEAddInEventsEx | A collection of AddInEvent objects. |
DISEAddInEventsEx2 | A collection of AddInEvent objects. |
DISEAnimationEvents | Animation events. |
DISEApplicationEvents | Fires application events. |
DISEApplicationWindowEvents | Provides access to the application window events. |
DISEAssemblyChangeEvents | Assembly change events. |
DISEAssemblyConfigurationChangeEvents | Fires AssemblyConfigurationChange user interface events. |
DISEAssemblyFamilyEvents | |
DISEAssemblyFamilyEvents2 | |
DISEAssemblyPhysicalPropertiesChangeEvents | Fires Assembly Physical Proeprties Change user interface events. |
DISEAssemblyRecomputeEvents | Represents a collection of assembly recompute events. |
DISEBeforeFileSaveAsEvents | Fires BeforeFileSaveAs user interface events. |
DISEBendTableEvents | Fires Bend Table events. |
DISECommand | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
DISECommandBarButtonEvents | A collection of CommandBarButtonEvent objects. |
DISECommandEvents | |
DISECommandWindowEvents | |
DISEDocumentEvents | Fires document events. |
DISEFeatureSelectedFromPFEvents | Feature selected from pathfinder Events. |
DISEFileUIEvents | Fires file user interface events. |
DISEhDCDisplayEvents | Fires display events. |
DISEMouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. |
DISEMouseEvents | |
DISESketchRecomputeEvents | Fires Sketch recompute events. |
DISEViewEvents | Fires view events. |
DisplayEvents | Fires display events. |
DividePartEvents | Represents a collection of DividedPart-based events. |
DocumentEvents | Fires document events. |
Documents | A collection of Document objects. |
DraftBendTableEvents | Contains the AfterUpdate event. |
DrawingViewEvents | Represents a collection of DrawingView events. |
Environment | The menus and accelerators to a Window object. Defines the set of commands that can be run while a window associated to an environment is active. |
Environments | A collection of Environment objects. |
FaceStyle | An object in the FaceStyles collection. |
FaceStyles | A collection of FaceStyle objects. |
FamilyOfPartsEvents | Represents a collection of Family of Parts events. |
FamilyOfPartsExEvents | |
FeatureLibraryEvents | Represents a collection of Feature Library-based events. |
FeatureSelectedFromPFEvents | These events are fired when a feature is selected from pathfinder. |
FileUIEvents | Fires file user interface events. |
FillStyle | Defines the fill characteristics of an enclosed object. |
FillStyles | A collection of FillStyle objects. |
GLDisplayEvents | Represents a collection of GLDisplay events. |
HatchPatternStyle | A vector pattern that is used to fill a closed boundary. |
HatchPatternStyles | A collection of HatchPatternStyle objects. |
HighlightSet | Represents an occurrence of a Highlight set in Assembly, Draft, Part, or Sheet Metal documents. |
HighlightSets | A collection of HighLightSet objects. |
IBiDMEvents | BiDM Events |
Insight | Automation users please note that, the "Insight Object" will not be supported from Solid Edge 2020 onwards, since we have stopped product support for "Solid Edge for Insight". |
InterDocumentUpdate | This interface will house methods for reporting, loading and saving the documents shown in the Component Tracker. |
InterpartLink | |
InterpartLinks | |
ISEAccelerator | Represents a collection of KeyBinding objects. |
ISEAccelerators | Represents a collection of Accelerator objects. |
ISEAddIn | A control that represents a command added to Solid Edge through the AddIn interface. |
ISEAddInEdgeBarEvents | |
ISEAddInEdgeBarEventsEx | |
ISEAddInEvents | A collection of AddInEvent objects. |
ISEAddInEventsEx | A collection of AddInEvent objects. |
ISEAddInEventsEx2 | A collection of AddInEvent objects. |
ISEAddInEx | A control that represents a command added to Solid Edge through the AddIn interface. |
ISEAddInEx2 | A control that represents a command added to Solid Edge through the AddIn interface. |
ISEAddIns | A collection of AddIn objects. |
ISEAddInSaveAsTranslator | An interface that allows an add-in to add save as capability for Solid Edge files. |
ISEAddInSaveAsTranslatorEvents | An interface that allows an add-in that has save as capability for Solid Edge files to respond to user interface events. |
ISEAnimationEvents | Animation events. |
ISEApplicationEvents | Fires application events. |
ISEApplicationEventsEx | Fires application events. |
ISEApplicationReadyEvents | Fires application is ready events. |
ISEApplicationV8AfterDocumentOpenEvent | Fires document open event |
ISEApplicationWindowEvents | Provides access to the application window events. |
ISEAssemblyChangeEvents | Assembly change events. |
ISEAssemblyConfigurationChangeEvents | Fires AssemblyConfigurationChange user interface events. |
ISEAssemblyFamilyEvents | |
ISEAssemblyFamilyEvents2 | |
ISEAssemblyPhysicalPropertiesChangeEvents | Fires Assembly Physical Proeprties Change user interface events. |
ISEAssemblyRecomputeEvents | Represents a collection of assembly recompute events. |
ISEBeforeFileSaveAsEvents | Fires BeforeFileSaveAs user interface events. |
ISEBendTableEvents | Fires Bend Table events. |
ISEBlockTableEvents | Contains the AfterUpdate event. |
ISECommand | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
ISECommandBar | Represents all menus, toolbars, and pop-up menus in Solid Edge. |
ISECommandBarButton | Represents buttons on toolbars and menus. |
ISECommandBarButtonEvents | A collection of CommandBarButtonEvent objects. |
ISECommandBarControl | Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects. |
ISECommandBarControls | Contains all of the buttons and pop-ups on a specific command bar. |
ISECommandBarPopup | Represents pop-ups on toolbars and menus. |
ISECommandBars | A collection of all of the command bars within a specific environment. |
ISECommandCategories | A collection of command categories |
ISECommandCategory | |
ISECommandEvents | |
ISECommandEx | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
ISECommandEx2 | Provides interfaces for Visual Basic users to capture user input to process Solid Edge events. |
ISECommandInfo | |
ISECommandInfoEx | |
ISECommandWindowEvents | |
ISEConnectorTableEvents | Contains the AfterUpdate event. |
ISEDividePartEvents | Represents a collection of DividedPart-based events. |
ISEDocumentEvents | Fires document events. |
ISEDraftBendTableEvents | Contains the AfterUpdate event. |
ISEDrawingViewEvents | Represents a collection of DrawingView events. |
ISEDynamicEditEvents | Fires dynamic edit events. |
ISEECEvents | SEEC Events |
ISEFamilyOfPartsEvents | Represents a collection of Family of Parts events. |
ISEFamilyOfPartsExEvents | |
ISEFeatureLibraryEvents | Represents a collection of Feature Library-based events. |
ISEFeatureSelectedFromPFEvents | Feature selected from pathfinder Events. |
ISEFileUIEvents | Fires file user interface events. |
ISEhDCDisplayEvents | Fires display events. |
ISEIGLDisplayEvents | Represents a collection of GLDisplay events. |
ISEKeyBinding | Provides information about an existing key binding. |
ISELocateFilterEvents | |
ISEModelRecomputeEvents | Fires model recompute events. |
ISEMouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. |
ISEMouseEvents | |
ISEMouseEx | |
ISEMouseEx2 | |
ISEMouseEx3 | |
ISENewFileUIEvents | |
ISEPartsListEvents | Contains the AfterUpdate event. |
ISEPhysicalPropertiesChangeEvents | Physical Properties change Events. |
ISERenderEvents | Represents a collection of rendering events. |
ISEShortCutMenuEvents | Event set for short-cut menu manipulations |
ISESketchRecomputeEvents | Fires Sketch recompute events. |
ISESPEvents | SESP Events |
ISEViewEvents | Fires view events. |
ISolidEdgeAddIn | Provides an interface for add-ins to implement for Solid Edge to connect to them. |
ISolidEdgeBar | |
ISolidEdgeBarEx | |
ISolidEdgeBarEx2 | |
ISolidEdgeCommandBar | |
ISolidEdgeRibbonBar | |
ISolidEdgeRibbonBarEx | |
KeyBinding | Provides information about an existing key binding. |
Layer | An object in the Layers collection object. |
Layers | A collection of Layer objects. |
LinearStyle | Consists of the information required to represent a line graphically. |
LinearStyles | A collection of LinearStyle objects. |
MatTable | |
ModelRecomputeEvents | Fires model recompute events. |
Mouse | Provides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events. |
NamedView | A Named View objects. |
NamedViews | Automation interface for IJNameMgr. |
NewFileUIEvents | |
PartsListEvents | Contains the AfterUpdate event. |
PhysicalPropertiesChangeEvents | Physical Properties change Events. |
Properties | A collection of Property objects. |
Property | A user-defined document attribute. |
PropertyEx | A user-defined document attribute. |
PropertySets | A collection of PropertySet objects. |
QueryObjects | Represents the collection of objects returned by a query. |
RadialMenu | |
Reference | Represents an object that references another object (a part or assembly, for example). |
RenderEvents | Represents a collection of rendering events. |
RibbonBar | |
RibbonBarControl | |
RibbonBarControls | |
RibbonBarGroup | |
RibbonBarGroups | |
RibbonBars | |
RibbonBarTab | |
RibbonBarTabs | |
RibbonBarTheme | |
RibbonBarThemes | |
RoutingSlip | Distributes a document to recipients either at one time or sequentially. |
SectionView | Automation object for a section view in a Part or Assembly document. |
SectionViews | Collection of section views. |
SEECEvents | SEEC Events |
SEGenericCollection | Represents a collection of AttachedProperty objects. |
SelectSet | A temporary grouping of one or more selected objects. |
Sensor | Represents an occurrence of a Sensor feature in an Assembly document, a Part document, or a Sheet Metal document. |
Sensors | A collection of Sensor objects. |
SESPEvents | SESP Events |
SheetMetalSensors | Represents a collection of sensors on a SheetMetalDocument. |
ShortcutMenuEvents | |
SketchRecomputeEvents | Fires Sketch recompute events. |
SolidEdgeDocument | |
SolidEdgeInsightXT | InsightXT Automation Object. |
SolidEdgeTCE | Solid Edge Teamcenter Automation object. |
SteeringWheel | Automation object for the Steering Wheel used in Sync Edit commands |
SummaryInfo | Contains information about a document. |
SwitchWindowCust | |
Symbol2d | Allows you to review or manipulate the symbol geometry, the attachment between a symbol and a source document, and the user property. |
SymbolProperties | A collection of SymbolProperty objects. |
Symbols | A collection of Symbol objects. |
TemplateManager | TemplateManager object to manage template documents and template lists |
TextCharStyle | Contains a set of character characteristics that can be applied as a set to the active text. |
TextCharStyles | A collection of TextCharStyle objects. |
TextStyle | Contains characteristics to apply to the active paragraph. |
TextStyles | A collection of TextStyle objects. |
UnitOfMeasure | The UnitOfMeasure object allows you to set and return the unit type and precision for each category, depending on the index of the unit. |
UnitsOfMeasure | Allows you to convert internal measurement units to user-specified measurement units. |
variable | Associates a name with a numeric value. |
VariableList | A list of Variable objects returned from a query. |
Variables | A collection of Variable objects. |
View | Provides methods and properties that allow you to manipulate Solid Edge window views. |
ViewEvents | Fires view events. |
ViewStyle | Contains a collection of properties that control view rendering. |
ViewStyles | A collection of ViewStyle objects. |
Window | Provides support for adjusting the size of the actual viewing area. |
Windows | A collection of Window objects. |