Class Module | Description |
---|---|
AdjustablePart | Adjustable part object. |
AFGrooveWeld | |
AFGrooveWelds | |
AngularRelation3d | A 3-D relation object. |
ArcSegment | Represents an occurrence of an ArcSegment element in an Assembly document. |
ArcSegments | Represents a collection of ArcSegment objects. |
AsmRefPlane | A planar object that provides a flat surface on which to create a profile within profile-based features. |
AsmRefPlanes | A collection of Assembly RefPlane objects. |
AssemblyBodies | |
AssemblyBody | |
AssemblyCopies | |
AssemblyCopy | |
AssemblyDocument | A document type used exclusively for assemblies. |
AssemblyDrivenPartFeatures | |
AssemblyDrivenPartFeaturesExtrudedCutout | |
AssemblyDrivenPartFeaturesExtrudedCutouts | |
AssemblyDrivenPartFeaturesHole | |
AssemblyDrivenPartFeaturesHoles | |
AssemblyDrivenPartFeaturesRevolvedCutout | |
AssemblyDrivenPartFeaturesRevolvedCutouts | |
AssemblyFamilyMember | Represents an occurrence of a member assembly in a family of assemblies. |
AssemblyFamilyMembers | Represents a collection of AssemblyFamilyMember objects. |
AssemblyFeatures | |
AssemblyFeaturesExtrudedCutout | |
AssemblyFeaturesExtrudedCutouts | |
AssemblyFeaturesExtrudedProtrusion | |
AssemblyFeaturesExtrudedProtrusions | |
AssemblyFeaturesHole | |
AssemblyFeaturesHoles | |
AssemblyFeaturesMirror | |
AssemblyFeaturesMirrors | |
AssemblyFeaturesPattern | |
AssemblyFeaturesPatterns | |
AssemblyFeaturesRevolvedCutout | |
AssemblyFeaturesRevolvedCutouts | |
AssemblyFeaturesRevolvedProtrusion | |
AssemblyFeaturesRevolvedProtrusions | |
AssemblyFeaturesSweptProtrusion | |
AssemblyFeaturesSweptProtrusions | |
AssemblyFilletWeld | |
AssemblyFilletWelds | |
AssemblyGroup | The AssemblyGroup object consists of methods that add components to or removes components from a group. |
AssemblyGroups | The AssemblyGroups object represents a collection of AssemblyGroup objects. |
AssemblyMirror | |
AssemblyMirrors | |
AssemblyPattern | Represents an assembly pattern. |
AssemblyPatternOccurrence | An assembly pattern occurrence. |
AssemblyPatterns | Represents a collection of AssemblyPattern objects. |
AssemblyProperties | Collection of AssemblyProperty objects. |
AssemblyProperty | Allows creation and manipulation of wiring attributes. |
AssemblyStitchWeld | |
AssemblyStitchWelds | |
AssemblyThread | |
AssemblyThreads | |
AxialRelation3d | Makes the cylindrical axis of a feature on one part colinear with the cylindrical axis of a feature on another part. |
Bundle | |
Bundles | |
Cable | |
Cables | |
CamFollowerRelation3d | Defines a cam-follower relationship between two objects. |
CenterPlaneRelation3d | Defines a center-plane relationship between objects. |
ComponentLayout | |
ComponentLayouts | |
Configuration | A set of assembly configuration settings. |
Configurations | Represents a collection of Configuration objects. |
CurveSegment | Represents an occurrence of a curve segment element. |
CurveSegments | Collection of CurveSegment objects. |
FastenerSystem | Represents Fastener System. |
FastenerSystems | Represents Fastener Systems. |
GearRelation3d | Defines a gear relationship between two objects. |
GroundRelation3d | Defines that a part remains fixed in its current position and orientation. |
Harness | |
Harnesses | |
ItemNumbers | |
Layout | An Assembly Layout object |
Layouts | Collection of Assembly Layouts. |
LineSegment | Represents an occurrence of a LineSegment element in an Assembly document. |
LineSegments | Represents a collection of LineSegment objects. |
Occurrence | An instance of an Occurrence or subassembly within an assembly. |
Occurrences | A collection of occurrence objects. |
Path | Represents an occurrence of a curve segment element. |
PathRelation3d | Defines a Path relationship between two objects. |
Paths | Collection of keypoint curve objects. |
PhysicalProperties | Contains the results of physical property calculations on the referenced object. |
Pipe | |
Pipes | |
PlanarRelation3d | Makes the planar face of a feature on one part parallel with the planar face of a feature on another part. |
PointRelation3d | An assembly 3-D point relation helper object. |
Queries | Represents a collection of Query objects. |
Query | Represents an instance of a Query on an associated AssemblyDocument object. |
Relations3d | A collection of relationships for parts and subassemblies that are contained in the referenced assembly. |
RigidSetRelation3d | |
SegmentAngularRelation3d | Represents an occurrence of an Segment Angular constraint in an Assembly document. |
SegmentDirectionRelation3d | Represents a relationship for which the specified relative orientations between constrained elements is maintained. |
SegmentDistanceRelation3d | Represents a relationship for which the distance between constrained elements is maintained. |
SegmentPointRelation3d | Represents a relationship for which the specified point relationship for a constrained element is maintained. |
SegmentRadiusRelation3d | Represents a relationship for which a specified radius is maintained for a constrained element. |
SegmentRelations3d | Represents a collection of all relationships applied to tubing segments within an AssemblyDocument object. |
Segments | Represents a collection of all segment-based objects (ex. LineSegment, ArcSegment) for the associated Assembly document. |
SegmentTangentRelation3d | Represents a relationship for which the specified tangency condition for constrained elements is maintained. |
SimplifiedAssemblies | Simplified Assemblies |
SimplifiedAssembly | Simplified Assembly |
Splice | |
Splices | |
StructuralFrame | The StructuralFrame object represents a structural frame constructed along path segments in an assembly document. |
StructuralFrames | The StructuralFrames object represents a collection of StructuralFrame objects. |
SubassemblyBodies | |
SubassemblyBody | |
SubOccurrence | An instance of an SubOccurrence or subassembly within an assembly. |
SubOccurrences | A collection of sub occurrence objects. |
TangentRelation3d | Defines a tangent relationship between two objects. |
TopologyReference | Represents an object that references a topological object (an edge or a face, for example). |
Tube | An object that encapsulates all tube-related information (for example, Tube path, material, bend radii, and wall thickness) in the associated Occurrence object. |
VirtualComponent | A virtual component object. |
VirtualComponentOccurrence | A virtual component occurrence object. |
VirtualComponentOccurrences | A collection of VirtualComponentOccurrence objects. |
Wire | |
WirePath | An occurrence of a wire path. |
WirePathCableMembers | Represents a collection of cable member WirePath objects. |
WirePaths | A collection of WirePath objects. |
WirePathSegments | Represents a collection of segment WirePath objects. |
WireRun | An occurrence of a wire run. |
WireRunPaths | Represents a collection of WireRun path objects. |
WireRuns | A collection of WireRun objects. |
Wires | |
Zone | The Zone object represents a zone in an assembly document. |
Zones | The Zones object returns a collection of all the zones defined for the assembly document. |
Enumeration | Description |
---|---|
AlternateAssemblyTypeConstants | Constants that describe what type of Alternate Assembly the assembly document is |
AssemblyBaseStylesConstants | Assembly Base Styles Constants |
AssemblyCopyActionConstants | |
AssemblyCopyComponentConstants | |
AssemblyCopyStatusConstants | |
AssemblyCopyTypeConstants | |
AssemblyFamilyMemberPropertyConstants | Assembly Family Member Property Constants |
AssemblyGlobalConstants | Assembly Global constants |
AssemblyPathfinderUpdateConstants | Assembly Pathfinder Update Constants |
AssemblyPatternTypeConstants | Constants that describe what type of Assembly Pattern |
AssemblyReportTypeConstants | Assembly Report Type Constants |
AssemblyWireHarnessReportTypeConstants | Assembly Wire Harness Report Type Constants |
ConfigurationTypeConstants | Configuration Type Constants |
ConstraintReplacementConstants | |
CurveSegmentPathAdditionStatusConstants | Curve Segment Path Addition Status Constants |
CurveSegmentPathRemovalStatusConstants | Curve Segment Path Removal Status Constants |
CurveSegmentValidationConstants | Curve Segment Validation Constants |
CurveSegmentWhichKeypointsConstants | Curve Segment Which Keypoints Constants |
HarnessSaveAsEcadStatusConstants | Harness Save As ECAD Status Constants |
HarnessTypeConstants | Harness Type Constants |
InterferenceStatusConstants | Interference Status constants |
ItemNumberModeConstants | |
MoveMultipleMoveTypeConstants | Move Multiple Move Type Constants |
MoveMultipleRelationshipConstants | Move Multiple Relationship Constants |
OccurrenceStatusConstants | Assembly Occurrence Status Constants |
PatternOffsetTypeConstants | Pattern Offset Type Constants |
PipeFittingEndTreatmentConstants | Pipe Fitting End Treatment Constants |
PipeFittingTypeConstants | Pipe Fitting Type Constants |
QueryConditionConstants | Query Condition Constants |
QueryPropertyConstants | Query Property Constants |
QueryScopeConstants | Query Scope Constants |
Relation3dDetailedStatusConstants | Assembly Relation3d Detailed Status Constants |
Relation3dGearRatioTypeConstants | Relation3d Gear Ratio Type Constants |
Relation3dGearTypeConstants | Relation3d Gear Type Constants |
Relation3dGeometryConstants | Assembly Relation3d Geometry Constants |
Relation3dOrientationConstants | Relation3d Orientation Constants |
Relation3dStatusConstants | Assembly Relation3d Status Constants |
seAssemblyBodyTypeConstants | Assembly Body Type Constants |
SegmentRelation3dDirectionConstants | Segment Relation3d Direction Constants |
SegmentRelation3dDistanceConstants | Segment Relation3d Distance Constants |
SegmentRelation3dGeometryConstants | Segment Relation3d Geometry Constants |
SegmentRelation3dStatusConstants | Segment Relation3d Status Constants |
SimplifiedAssemblyMode | Defines the whether the particular document has modeled or visible simplification |
StructuralFrameEndConditionConstants | Structural Frame End Condition Constants |
TubePropertyPidConstants | Tube Property Pid Constants |
TubeSegmentAdditionStatusConstants | Tube Segment Addition Status Constants |
TubeSegmentRemovalStatusConstants | Tube Segment Removal Status Constants |
UpdateStructureCacheConstants | Update Structure Cache Constants |
VirtualComponentPublishConstants | Virtual Component Publish Constants |
VirtualComponentStatusConstants | Virtual Component Status Constants |
VirtualComponentTypeConstants | Virtual Component Type Constants |
VisibilityBasedSimplifiedAssemblyCopyType | Defines the whether faces or bodies are copied to the simplified assembly representation after visibility processing |
WirePathConstants | Wire Path Constants |