Solid Edge Assembly Type Library
WireRun Object
Members 
Description
An occurrence of a wire run.
Object Model
WireRun ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionOccurrence ObjectAdjustablePart ObjectTube ObjectAdjustablePart ObjectSubassemblyBodies CollectionSubOccurrences CollectionAssemblyDocument ObjectWireRunPaths Collection
Remarks
The WireRun object can be used to generate a WireFeature object in a part file.
See Also

WireRun Members