Solid Edge Assembly Type Library
Paths Collection
Members 
Description
Collection of keypoint curve objects.
Example
Imports System.Runtime.InteropServices
Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApp As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim paths As SolidEdgeAssembly.Paths = Nothing
        Dim path As SolidEdgeAssembly.Path = Nothing
        Dim x As Integer
        Dim name As String
        Dim pointtypes(1) As SolidEdgeConstants.PointTypeConstants
        Dim points(5) As Double
        Dim edgeset(1) As Object
        Dim pointtyp(1) As SolidEdgeConstants.KeyPointType

        Dim obj1Ref1 As Object
        Dim objFirstPart As SolidEdgeAssembly.Occurrence

        Dim objVer1 As SolidEdgeGeometry.Vertex
        Dim face1 As SolidEdgeGeometry.Edge
        Dim extprot As SolidEdgePart.ExtrudedProtrusion
        Dim leng As Double
        Dim arraydouble(5) As Double

        Try
            objApp = Marshal.GetActiveObject("SolidEdge.Application")
            If objApp Is Nothing Then
                objApp = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
                objApp.Visible = True
            End If
            'Asm1.asm is a simple assembly having a cube in it
            objDoc = objApp.Documents.Open("c:\asm1.asm")

            paths = objDoc.Paths
            x = paths.Count()

            pointtypes(0) = SolidEdgeConstants.PointTypeConstants.igKeyPoint
            pointtypes(1) = SolidEdgeConstants.PointTypeConstants.igSpacePoint

            points(0) = 0
            points(1) = 0
            points(2) = 0.01
            points(3) = 0
            points(4) = 0.01
            points(5) = 0.01

            objFirstPart = objDoc.Occurrences.Item(1)


            extprot = objFirstPart.PartDocument.Models(1).ExtrudedProtrusions(1)
            face1 = extprot.BottomCap.Edges(1)
            objVer1 = face1.StartVertex
            obj1Ref1 = objDoc.CreateReference(objFirstPart, objVer1)

            edgeset(0) = obj1Ref1

            path = paths.Add(2, pointtypes, edgeset, pointtyp, points, _
                             SolidEdgePart.KeypointEndConditionConstants.seKeypointEndConditionNatural, _
                             SolidEdgePart.KeypointEndConditionConstants.seKeypointEndConditionNatural)
            
            path.GetLength(leng)
            path.GetEndPoints(arraydouble)
            name = path.Name
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

Paths Members  | Solid Edge V18 - What's New