Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldPrepareEdges |
WeldPrepareEdges.COMPLEX
Same as entire edge, but use if a portion of target body is below the desired weld
|
static WeldPrepareEdges |
WeldPrepareEdges.ENTIRE_EDGE
Output edges will be prepared for entire edge length
|
static WeldPrepareEdges |
WeldPrepareEdges.NONE
Output edges will not be prepared
|
static WeldPrepareEdges |
WeldPrepareEdges.WELD_LIMITS
Output edges will be prepared for the weld length only
|
Modifier and Type | Method and Description |
---|---|
WeldPrepareEdges |
GrooveBuilder.prepareEdges()
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.prepareEdges() and WeldGrooveBuilder.setPrepareEdges(nxopen.weld.WeldGrooveBuilder.Prepare) instead.
|
static WeldPrepareEdges |
WeldPrepareEdges.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPrepareEdges |
WeldPrepareEdges.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPrepareEdges[] |
WeldPrepareEdges.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GrooveBuilder.setPrepareEdges(WeldPrepareEdges prepareEdges)
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.prepareEdges() and WeldGrooveBuilder.setPrepareEdges(nxopen.weld.WeldGrooveBuilder.Prepare) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.