public class WeldPrepareEdges extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COMPLEX
Same as entire edge, but use if a portion of target body is below the desired weld
|
static int |
_ENTIRE_EDGE
Output edges will be prepared for entire edge length
|
static int |
_NONE
Output edges will not be prepared
|
static int |
_WELD_LIMITS
Output edges will be prepared for the weld length only
|
static WeldPrepareEdges |
COMPLEX
Same as entire edge, but use if a portion of target body is below the desired weld
|
static WeldPrepareEdges |
ENTIRE_EDGE
Output edges will be prepared for entire edge length
|
static WeldPrepareEdges |
NONE
Output edges will not be prepared
|
static WeldPrepareEdges |
WELD_LIMITS
Output edges will be prepared for the weld length only
|
Modifier and Type | Method and Description |
---|---|
static WeldPrepareEdges |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPrepareEdges |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPrepareEdges[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldPrepareEdges NONE
public static final WeldPrepareEdges ENTIRE_EDGE
public static final WeldPrepareEdges WELD_LIMITS
public static final WeldPrepareEdges COMPLEX
public static final int _NONE
public static final int _ENTIRE_EDGE
public static final int _WELD_LIMITS
public static final int _COMPLEX
public static WeldPrepareEdges valueOf(int value)
public static WeldPrepareEdges valueOf(String name)
public static WeldPrepareEdges[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.