Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Interface and Description |
---|---|
interface |
JointExitBuilder
Used to set custom edge preparation parameters of a
WeldJoint feaure. |
Modifier and Type | Method and Description |
---|---|
WeldJointBuilder |
WeldManager.createJointBuilder(WeldJoint weldJoint)
Creates a
WeldJointBuilder
License requirements: structure_weld ("STRUCTURE WELD") Created in NX8.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
CustomManager.VariableBevelHandler.variableBevelHandler(WeldJointBuilder jointBuilder,
Curve jointCurve)
User defined method that returns the angle divisions for a variable bevel.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.