Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.ANGLE
At specifed angle.
|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.COMPUTED_ANGLE
At angle computed from geometry and tables.
|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.EQUAL_SEGMENTS
Specified number of equal segments.
|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.LENGTH
At equal arc length.
|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.LIMITS
At limits defined by
WeldJointBuilder.limitList() . |
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.NONE
No split.
|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.SKIP
Skip joint.
|
Modifier and Type | Method and Description |
---|---|
WeldJointBuilder.SplitTypes |
WeldJointBuilder.splitOption()
Returns the method used to split the joint
License requirements: None. |
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.SplitTypes |
WeldJointBuilder.SplitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.SplitTypes[] |
WeldJointBuilder.SplitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldJointBuilder.setSplitOption(WeldJointBuilder.SplitTypes option)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.