Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldJointBuilder.DestinationTypes |
WeldJointBuilder.DestinationTypes.NEW_COMPONENT
Create a new componenent for each joint under the work part.
|
static WeldJointBuilder.DestinationTypes |
WeldJointBuilder.DestinationTypes.WORK_PART
Create new joints in work part.
|
Modifier and Type | Method and Description |
---|---|
WeldJointBuilder.DestinationTypes |
WeldJointBuilder.destination()
Returns the destination to create new joints
License requirements: None. |
static WeldJointBuilder.DestinationTypes |
WeldJointBuilder.DestinationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.DestinationTypes |
WeldJointBuilder.DestinationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.DestinationTypes[] |
WeldJointBuilder.DestinationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldJointBuilder.setDestination(WeldJointBuilder.DestinationTypes type)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.