Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldJointBuilder.CoordinateSystem |
WeldJointBuilder.CoordinateSystem.ABSOLUTE
Desired points and vectors should be in absolute coordinates.
|
static WeldJointBuilder.CoordinateSystem |
WeldJointBuilder.CoordinateSystem.SHIP
Desired points and vectors should be in ship coordinate system.
|
Modifier and Type | Method and Description |
---|---|
static WeldJointBuilder.CoordinateSystem |
WeldJointBuilder.CoordinateSystem.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.CoordinateSystem |
WeldJointBuilder.CoordinateSystem.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.CoordinateSystem[] |
WeldJointBuilder.CoordinateSystem.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
WeldJointBuilder.MidPointInformationData |
WeldJointBuilder.getMidPointInformation(WeldJointBuilder.CoordinateSystem desiredCoordinateSystem)
Gets the joint curve mid point, tangent, and face normals at the mid point from the primary and secondary bodies.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.