Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldJointBuilder.Application |
WeldJointBuilder.Application.ROUTING
Routing Application.
|
static WeldJointBuilder.Application |
WeldJointBuilder.Application.STRUCTURE_WELDING
Structure Welding Application.
|
Modifier and Type | Method and Description |
---|---|
WeldJointBuilder.Application |
WeldJointBuilder.createdApplication()
Returns the application where joint is created
License requirements: None. |
static WeldJointBuilder.Application |
WeldJointBuilder.Application.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.Application |
WeldJointBuilder.Application.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.Application[] |
WeldJointBuilder.Application.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldJointBuilder.setCreatedApplication(WeldJointBuilder.Application application)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.