Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldBeadBuilder.FaceInferMethodType |
WeldBeadBuilder.FaceInferMethodType.NONE
only use selected faces to create the bead path curve
|
static WeldBeadBuilder.FaceInferMethodType |
WeldBeadBuilder.FaceInferMethodType.TANGENT_FACES
use faces tangent to selected faces to create the bead path curve
|
Modifier and Type | Method and Description |
---|---|
WeldBeadBuilder.FaceInferMethodType |
WeldBeadBuilder.faceInferMethod()
Returns the method to use when inferring faces to create the bead guide curve path.
|
static WeldBeadBuilder.FaceInferMethodType |
WeldBeadBuilder.FaceInferMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBeadBuilder.FaceInferMethodType |
WeldBeadBuilder.FaceInferMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBeadBuilder.FaceInferMethodType[] |
WeldBeadBuilder.FaceInferMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldBeadBuilder.setFaceInferMethod(WeldBeadBuilder.FaceInferMethodType faceInferMethod)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.