public static class WeldBeadBuilder.FaceInferMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
only use selected faces to create the bead path curve
|
static int |
_TANGENT_FACES
use faces tangent to selected faces to create the bead path curve
|
static WeldBeadBuilder.FaceInferMethodType |
NONE
only use selected faces to create the bead path curve
|
static WeldBeadBuilder.FaceInferMethodType |
TANGENT_FACES
use faces tangent to selected faces to create the bead path curve
|
Modifier and Type | Method and Description |
---|---|
static WeldBeadBuilder.FaceInferMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBeadBuilder.FaceInferMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBeadBuilder.FaceInferMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldBeadBuilder.FaceInferMethodType TANGENT_FACES
public static final WeldBeadBuilder.FaceInferMethodType NONE
public static final int _TANGENT_FACES
public static final int _NONE
public static WeldBeadBuilder.FaceInferMethodType valueOf(int value)
public static WeldBeadBuilder.FaceInferMethodType valueOf(String name)
public static WeldBeadBuilder.FaceInferMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.