Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Interface and Description |
---|---|
interface |
PointMarkPointBuilder
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use PointMarkBuilder.newPointsOverride() Created in NX10.0.0 |
Modifier and Type | Method and Description |
---|---|
JointmarkPointsBuilder |
JointmarkPointsBuilderList.findItem(int index)
Returns the object at the input index.
|
JointmarkPointsBuilder[] |
JointmarkPointsBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
JointmarkPointsBuilder |
JointmarkBuilder.newPoints()
Creates a
JointmarkPointsBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
JointmarkPointsBuilderList.append(JointmarkPointsBuilder object)
Appends an object to the list
License requirements: None. |
void |
JointmarkPointsBuilderList.append(JointmarkPointsBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
JointmarkPointsBuilderList.erase(JointmarkPointsBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
JointmarkPointsBuilderList.erase(JointmarkPointsBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
JointmarkPointsBuilderList.findIndex(JointmarkPointsBuilder obj)
Finds the index where the input object appears.
|
void |
JointmarkPointsBuilderList.insert(int location,
JointmarkPointsBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
JointmarkPointsBuilderList.setContents(JointmarkPointsBuilder[] objects)
Sets the contents of the entire list.
|
void |
JointmarkPointsBuilderList.swap(JointmarkPointsBuilder object1,
JointmarkPointsBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.