public interface PointMarkBuilder extends JointmarkBuilder
PointMark
feature. WeldManager.createPointMarkBuilder(nxopen.weld.PointMark)
Property | Value |
---|---|
Associativity | 1 |
ConnectPart | 0 |
ConstructionMethod | GuideCurve |
CreateSingleFeatures | 0 |
OrientationMethod | SurfaceNormal |
ReferenceSheetType | Overlap |
ReuseFeaturesMethod | SameConnectingParts |
ShowWorkCsys | 1 |
Modifier and Type | Interface and Description |
---|---|
static class |
PointMarkBuilder.WeldTypes
The weld type to create.
|
JointmarkBuilder.ConnectedPanelTypes, JointmarkBuilder.FromReuseFeaturesData, JointmarkBuilder.Method, JointmarkBuilder.OrientationMethodTypes, JointmarkBuilder.ProjectionDirectionOptions, JointmarkBuilder.ReferenceSheetTypes, JointmarkBuilder.ReuseMethod
Modifier and Type | Method and Description |
---|---|
void |
appendPointsOverride(boolean create)
Creates a list of points on the overlap sheet.
|
PointMarkPointBuilder |
newPointsOverride()
Creates a
PointMarkPointBuilder object. |
void |
setShowSolids(boolean showSolids)
License requirements: ugweld ("UG WELD") . |
void |
setWeldType(PointMarkBuilder.WeldTypes weldType)
License requirements: ugweld ("UG WELD") . |
boolean |
showSolids()
Returns the display mode.
|
PointMarkBuilder.WeldTypes |
weldType()
Returns the weld type references in the customer defaults to create.
|
appendPoints, askConnectedFaces, associativity, characteristics, connectedPanelType, connectPart, constructionMethod, createReferenceData, createSingleFeatures, createSymbolCurve, deleteReferenceData, distanceTolerance, faceSetsList, fixedCsys, fromReuseFeatures, getCreateReferenceDataMessages, getReferenceSheet, getSelectedReferences, getSheetEdges, guideCurvesList, mapFeaturesToPoints, moveReferenceSheet, newFaceSets, newGuide, newPoints, notifyIfParentPointMoved, orientationMethod, plane, pointList, projectionDirectionOption, rediscoverFaces, referenceSheetType, reuseFeatures, reuseFeaturesMethod, selectMirrorObject, selectPointsObject, selectTranslateObject, setAssociativity, setConnectedPanelType, setConnectPart, setConstructionMethod, setCreateSingleFeatures, setDisplayCsys, setDistanceTolerance, setFixedCsys, setNotifyIfParentPointMoved, setOrientationMethod, setPlane, setProjectionDirectionOption, setReferenceSheetType, setReuseFeaturesMethod, setShowThruState, setShowWorkCsys, setTranslateCsys, setVector, showWorkCsys, translateCsys, translateX, translateY, translateZ, updateFeatures, updatePoint, updateReferenceSheet, vector
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
PointMarkBuilder.WeldTypes weldType() throws NXException, RemoteException
NXException
RemoteException
void setWeldType(PointMarkBuilder.WeldTypes weldType) throws NXException, RemoteException
weldType
- NXException
RemoteException
PointMarkPointBuilder newPointsOverride() throws NXException, RemoteException
PointMarkPointBuilder
object.
NXException
RemoteException
void appendPointsOverride(boolean create) throws NXException, RemoteException
create
- Create or EditNXException
RemoteException
boolean showSolids() throws NXException, RemoteException
NXException
RemoteException
void setShowSolids(boolean showSolids) throws NXException, RemoteException
showSolids
- true- Show Weld.PointMarkPoint features in solid mode. fale- show in point mode.NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.