Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
JointItemBuilder[] |
WeldJointBuilder.NewlyCreatedJointsData.newitembuilder |
Modifier and Type | Method and Description |
---|---|
JointItemBuilder |
JointItemBuilderList.findItem(int index)
Returns the object at the input index.
|
JointItemBuilder[] |
JointItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
JointItemBuilder |
WeldJointBuilder.getSingleJoint(Curve curve)
Gets the
JointItemBuilder object associated to the input curve. |
JointItemBuilder |
WeldJointBuilder.newItem()
Creates a
JointItemBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
JointItemBuilderList.append(JointItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
JointItemBuilderList.append(JointItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
JointItemBuilderList.erase(JointItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
JointItemBuilderList.erase(JointItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
JointItemBuilderList.findIndex(JointItemBuilder obj)
Finds the index where the input object appears.
|
void |
JointItemBuilderList.insert(int location,
JointItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
CustomManager.PipeJointSetType.pipeJointSetType(JointItemBuilder joint)
User defined method that is called whenever a welding joint is created.
|
void |
JointItemBuilderList.setContents(JointItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
JointItemBuilderList.swap(JointItemBuilder object1,
JointItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.