Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.EnumFillFaceHolesType.BOTH |
static FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.EnumFillFaceHolesType.NONE |
static FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.EnumFillFaceHolesType.SET1 |
static FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.EnumFillFaceHolesType.SET2 |
Modifier and Type | Method and Description |
---|---|
FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.fillFaceHoles()
Returns the value to identify if the face set should be filled during construction.
|
static FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.EnumFillFaceHolesType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FilletBuilder.EnumFillFaceHolesType |
FilletBuilder.EnumFillFaceHolesType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FilletBuilder.EnumFillFaceHolesType[] |
FilletBuilder.EnumFillFaceHolesType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FilletBuilder.setFillFaceHoles(FilletBuilder.EnumFillFaceHolesType fillFaceHolesType)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.