Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static DatumCommonBuilder.CreationDirectionMethods |
DatumCommonBuilder.CreationDirectionMethods.DEFAULT
Use the default construction method
|
static DatumCommonBuilder.CreationDirectionMethods |
DatumCommonBuilder.CreationDirectionMethods.OPPOSITE
Reverse the construction orientation
|
Modifier and Type | Method and Description |
---|---|
DatumCommonBuilder.CreationDirectionMethods |
DatumCommonBuilder.creationDirection()
Returns the creation direction.
|
static DatumCommonBuilder.CreationDirectionMethods |
DatumCommonBuilder.CreationDirectionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumCommonBuilder.CreationDirectionMethods |
DatumCommonBuilder.CreationDirectionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumCommonBuilder.CreationDirectionMethods[] |
DatumCommonBuilder.CreationDirectionMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumCommonBuilder.setCreationDirection(DatumCommonBuilder.CreationDirectionMethods creationDirection)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.