public static class DatumCommonBuilder.CreationDirectionMethods extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT
Use the default construction method
|
static int |
_OPPOSITE
Reverse the construction orientation
|
static DatumCommonBuilder.CreationDirectionMethods |
DEFAULT
Use the default construction method
|
static DatumCommonBuilder.CreationDirectionMethods |
OPPOSITE
Reverse the construction orientation
|
Modifier and Type | Method and Description |
---|---|
static DatumCommonBuilder.CreationDirectionMethods |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumCommonBuilder.CreationDirectionMethods |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumCommonBuilder.CreationDirectionMethods[] |
values()
Returns an array that contains the values for this enum.
|
public static final DatumCommonBuilder.CreationDirectionMethods DEFAULT
public static final DatumCommonBuilder.CreationDirectionMethods OPPOSITE
public static final int _DEFAULT
public static final int _OPPOSITE
public static DatumCommonBuilder.CreationDirectionMethods valueOf(int value)
public static DatumCommonBuilder.CreationDirectionMethods valueOf(String name)
public static DatumCommonBuilder.CreationDirectionMethods[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.