Package | Description |
---|---|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Field and Description |
---|---|
static XmlComparator.Result |
XmlComparator.Result.DIFFERENT
Represents two xml files are different
|
static XmlComparator.Result |
XmlComparator.Result.IDENTICAL
Represents two xml files are identical
|
Modifier and Type | Method and Description |
---|---|
XmlComparator.Result |
XmlComparator.compareXmlFiles(String workXmlFile,
String masterXmlFile,
XmlComparator.Options compareOptions)
Compares two xml format files.
|
static XmlComparator.Result |
XmlComparator.Result.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static XmlComparator.Result |
XmlComparator.Result.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static XmlComparator.Result[] |
XmlComparator.Result.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.