public static class XmlComparator.Result extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIFFERENT
Represents two xml files are different
|
static int |
_IDENTICAL
Represents two xml files are identical
|
static XmlComparator.Result |
DIFFERENT
Represents two xml files are different
|
static XmlComparator.Result |
IDENTICAL
Represents two xml files are identical
|
Modifier and Type | Method and Description |
---|---|
static XmlComparator.Result |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static XmlComparator.Result |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static XmlComparator.Result[] |
values()
Returns an array that contains the values for this enum.
|
public static final XmlComparator.Result IDENTICAL
public static final XmlComparator.Result DIFFERENT
public static final int _IDENTICAL
public static final int _DIFFERENT
public static XmlComparator.Result valueOf(int value)
public static XmlComparator.Result valueOf(String name)
public static XmlComparator.Result[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.