Package | Description |
---|---|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Field and Description |
---|---|
static RequirementCheck.SaveResultsToTeamcenterOptions |
RequirementCheck.SaveResultsToTeamcenterOptions.ALWAYS_SAVE
Always perform save
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
RequirementCheck.SaveResultsToTeamcenterOptions.DO_NOT_SAVE
Do not perform save.
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
RequirementCheck.SaveResultsToTeamcenterOptions.SAVE_IF_PASSED
Perform save only if the result is passed.
|
Modifier and Type | Method and Description |
---|---|
RequirementCheck.SaveResultsToTeamcenterOptions |
RequirementCheck.saveResultsToTeamcenterOption()
Returns the Save Results to Teamcenter option
License requirements: None. |
static RequirementCheck.SaveResultsToTeamcenterOptions |
RequirementCheck.SaveResultsToTeamcenterOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
RequirementCheck.SaveResultsToTeamcenterOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RequirementCheck.SaveResultsToTeamcenterOptions[] |
RequirementCheck.SaveResultsToTeamcenterOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RequirementCheck.setSaveResultsToTeamcenterOption(RequirementCheck.SaveResultsToTeamcenterOptions option)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.