public static class RequirementCheck.SaveResultsToTeamcenterOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALWAYS_SAVE
Always perform save
|
static int |
_DO_NOT_SAVE
Do not perform save.
|
static int |
_SAVE_IF_PASSED
Perform save only if the result is passed.
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
ALWAYS_SAVE
Always perform save
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
DO_NOT_SAVE
Do not perform save.
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
SAVE_IF_PASSED
Perform save only if the result is passed.
|
Modifier and Type | Method and Description |
---|---|
static RequirementCheck.SaveResultsToTeamcenterOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RequirementCheck.SaveResultsToTeamcenterOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RequirementCheck.SaveResultsToTeamcenterOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final RequirementCheck.SaveResultsToTeamcenterOptions DO_NOT_SAVE
public static final RequirementCheck.SaveResultsToTeamcenterOptions SAVE_IF_PASSED
public static final RequirementCheck.SaveResultsToTeamcenterOptions ALWAYS_SAVE
public static final int _DO_NOT_SAVE
public static final int _SAVE_IF_PASSED
public static final int _ALWAYS_SAVE
public static RequirementCheck.SaveResultsToTeamcenterOptions valueOf(int value)
public static RequirementCheck.SaveResultsToTeamcenterOptions valueOf(String name)
public static RequirementCheck.SaveResultsToTeamcenterOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.