Package | Description |
---|---|
nxopen.userdefinedobjects |
Provides classes and interfaces for User Defined Objects (UDOs).
|
Modifier and Type | Method and Description |
---|---|
UserDefinedObject.LinkDefinition[] |
UserDefinedObject.getLinks(UserDefinedObject.LinkType linkType)
Gets all links with the given link type that are stored with this UDO
License requirements: None. |
UserDefinedObject.LinkDefinition[] |
UserDefinedObject.getLinks(UserDefinedObject.LinkType linkType,
int offset,
int length)
Gets the links with the given link type that are stored in the specified range with this UDO
License requirements: None. |
UserDefinedObject.LinkDefinition[] |
UserDefinedObject.popLinks(UserDefinedObject.LinkType linkType,
int numLinks)
Removes the links stored at the end of the given link type's link array for this UDO,
and returns them in an array
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
UserDefinedObject.pushLinks(UserDefinedObject.LinkType linkType,
UserDefinedObject.LinkDefinition[] links)
Add the specified links to the end of the given link type's link array for this UDO
License requirements: None. |
void |
UserDefinedObject.setLinks(UserDefinedObject.LinkType linkType,
int offset,
int length,
UserDefinedObject.LinkDefinition[] links)
Replaces the links of the given link type stored with this UDO in the specified range with a new array of links
License requirements: None. |
void |
UserDefinedObject.setLinks(UserDefinedObject.LinkType linkType,
UserDefinedObject.LinkDefinition[] links)
Sets all of the links with the given link type stored with this UDO.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.