Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.userdefinedobjects |
Provides classes and interfaces for User Defined Objects (UDOs).
|
Modifier and Type | Method and Description |
---|---|
boolean |
Selection.getSelectionStatusOfUserDefinedClass(UserDefinedClass udoClass)
Gets whether or not the user defined class is available for selection.
|
void |
Selection.setSelectionStatusOfUserDefinedClass(UserDefinedClass udoClass,
boolean selectionStatus)
Sets whether or not the user defined class is available for selection.
|
Modifier and Type | Method and Description |
---|---|
UserDefinedClass |
UserDefinedObjectFeatureBuilder.userDefinedClass()
Returns the associated UserDefinedClass, Note the class is ignored if there is a valid UDO specified.
|
Modifier and Type | Method and Description |
---|---|
void |
UserDefinedObjectFeatureBuilder.setUserDefinedClass(UserDefinedClass udoClass)
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
UserDefinedClass |
UserDefinedClassManager.createUserDefinedObjectClass(String className,
String friendlyName)
Constructs a new
UserDefinedClass object. |
UserDefinedClass |
UserDefinedClassManager.getUserDefinedClassFromClassName(String className)
Get the
UserDefinedClass object associated with the given class name. |
UserDefinedClass |
UserDefinedClassManager.newUserDefinedClass()
Creats a new UserDefinedClass object
License requirements: None. |
UserDefinedClass |
UserDefinedObject.userDefinedClass()
Returns the
UserDefinedClass for this UDO
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
UserDefinedObject |
UserDefinedObjectManager.createUserDefinedObject(UserDefinedClass udoClass)
Constructs a new
UserDefinedObjectFeature . |
UserDefinedObject[] |
UserDefinedObjectManager.getUdosOfClass(UserDefinedClass udoClass)
Finds all
UserDefinedObject instances that use the given UserDefinedClass . |
void |
UserDefinedObject.setUserDefinedClass(UserDefinedClass userDefinedClass)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.