Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Method and Description |
---|---|
void |
UpdateFormboardBuilder.setHarnesses(HarnessDevice[] harnesses)
Sets the harnesses within the harness part that the formboard must be
compared with.
|
void |
FormboardManager.storeHarnessesToFlatten(HarnessDevice[] harnesses)
Examines the input list of harnesses and stores information from the harnesses into the part containing
this
FormboardManager . |
Modifier and Type | Field and Description |
---|---|
HarnessDevice |
RouteManager.SearchCriteria.owningHarness
Optional.
|
Modifier and Type | Method and Description |
---|---|
HarnessDevice |
Stock.getHarnessDevice()
For Routing Electrical application only, returns the
HarnessDevice
that owns the wire or wires that make up a stock bundle. |
Modifier and Type | Method and Description |
---|---|
boolean |
CustomManager.ValidateFormboardPlugin.validateFormboardPlugin(HarnessDevice[] harnesses)
This defines the prototype for the validate formboard plugin.
|
Constructor and Description |
---|
SearchCriteria(RouteManager.FindObjectType objectTypeInitial,
HarnessDevice owningHarnessInitial,
String applicationNameInitial,
String uniqueIDInitial)
Constructor for the SearchCriteria object.
|
Modifier and Type | Interface and Description |
---|---|
interface |
SystemDevice
The Electrical SystemDevice corresponds to a system instance of the
SingleDevice . |
Modifier and Type | Method and Description |
---|---|
HarnessDevice |
HarnessDeviceCollection.createHarnessDevice()
Creates
HarnessDevice . |
HarnessDevice |
HarnessDeviceCollection.createHarnessDevice(String harnessName)
Creates
HarnessDevice with given name. |
HarnessDevice |
ElectricalStockDevice.findNearestHarnessDevice()
Find the nearest
HarnessDevice encountered up the parent-child hierarchy. |
HarnessDevice |
ConnectorDevice.findNearestHarnessDevice()
Get the nearest
HarnessDevice encountered up the parent-child hierarchy. |
HarnessDevice |
Connection.findNearestHarnessDevice()
Query this connection to find the nearest harness.
|
HarnessDevice[] |
HarnessDeviceCollection.getHarnessSingleDevices()
Get harnesses
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Modifier and Type | Method and Description |
---|---|
void |
ElectricalStockDevice.changeHarness(HarnessDevice harnessDevice)
Adds this stockdevice as child of given HarnessDevice.
|
ConnectorDevice |
ConnectorDeviceCollection.createConnectorDevice(HarnessDevice harnessDevice,
String equipmentName,
String connectorName,
ConnectorDevice.ComponentType connectorType)
Finds or Creates a
ConnectorDevice for given equipmentName and or
connectorName. |
boolean |
ConnectorDevice.isNxConnector(HarnessDevice elecHarnessDevice)
Is the device a connector?
|
boolean |
ConnectorDevice.isNxDevice(HarnessDevice elecHarnessDevice)
Is the device a NX device?
|
boolean |
ConnectorDevice.isUsedInRoutedConnection(HarnessDevice elecHarnessDevice)
Is the device used in a routed connection?
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.