Package | Description |
---|---|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Field and Description |
---|---|
static Connection.RouteLevel |
Connection.RouteLevel.COMPONENT
Route to the connector component directly without regard for the pins.
|
static Connection.RouteLevel |
Connection.RouteLevel.MIXED
Route to the pin, if possible, otherwise route to the component.
|
static Connection.RouteLevel |
Connection.RouteLevel.NOT_ROUTED |
static Connection.RouteLevel |
Connection.RouteLevel.PIN
Route to the pin on the connector component.
|
Modifier and Type | Method and Description |
---|---|
Connection.RouteLevel |
Connection.getRoutedLevelEnum()
Similar to
Connection.getRoutedLevel() ,
but returns the Connection.RouteLevel enumeration instead of a string. |
static Connection.RouteLevel |
Connection.RouteLevel.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Connection.RouteLevel |
Connection.RouteLevel.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Connection.RouteLevel[] |
Connection.RouteLevel.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Connection.assignPath(Connection.RouteLevel routeLevel,
Path path)
Assigns the given path to this connection and routes the connection on the path using the given routing level.
|
void |
Connection.automaticallyRoute(Connection.RouteLevel routeLevel)
Automatically routes this connection on the shortest path using the given routing level.
|
Path[] |
Connection.findPaths(Connection.RouteLevel routeLevel)
Returns all the possible paths this connection can use.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.