public static class Connection.RouteLevel extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COMPONENT
Route to the connector component directly without regard for the pins.
|
static int |
_MIXED
Route to the pin, if possible, otherwise route to the component.
|
static int |
_NOT_ROUTED |
static int |
_PIN
Route to the pin on the connector component.
|
static Connection.RouteLevel |
COMPONENT
Route to the connector component directly without regard for the pins.
|
static Connection.RouteLevel |
MIXED
Route to the pin, if possible, otherwise route to the component.
|
static Connection.RouteLevel |
NOT_ROUTED |
static Connection.RouteLevel |
PIN
Route to the pin on the connector component.
|
Modifier and Type | Method and Description |
---|---|
static Connection.RouteLevel |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Connection.RouteLevel |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Connection.RouteLevel[] |
values()
Returns an array that contains the values for this enum.
|
public static final Connection.RouteLevel NOT_ROUTED
public static final Connection.RouteLevel PIN
public static final Connection.RouteLevel COMPONENT
public static final Connection.RouteLevel MIXED
public static final int _NOT_ROUTED
public static final int _PIN
public static final int _COMPONENT
public static final int _MIXED
public static Connection.RouteLevel valueOf(int value)
public static Connection.RouteLevel valueOf(String name)
public static Connection.RouteLevel[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.