Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.BEZIER
The defining type represents a G1-continuous, piecewise cubic Bezier.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.BEZIER_MAX_CURVATURE
The defining type represents a G1-continuous, piecewise cubic Bezier with bounded maximum curvature.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.BEZIER_SLACK
The defining type represents a G1-continuous, piecewise cubic Bezier with pseudo gravity slack.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.INTERPOLATION
The defining type represents a C1-continuous, interpolation spline.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.PARAMETRIC
The defining type represents a G1-continuous, parametric curve.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.UNSUPPORTED
The defining type is unsupported.
|
Modifier and Type | Method and Description |
---|---|
SplinePathBuilder.DefiningTypes |
SplinePathBuilder.definingType()
Returns the type which specifies the shape of the spline.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.DefiningTypes |
SplinePathBuilder.DefiningTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.DefiningTypes[] |
SplinePathBuilder.DefiningTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SplinePathBuilder.setDefiningType(SplinePathBuilder.DefiningTypes definingType)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.