public static class SplinePathBuilder.DefiningTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BEZIER
The defining type represents a G1-continuous, piecewise cubic Bezier.
|
static int |
_BEZIER_MAX_CURVATURE
The defining type represents a G1-continuous, piecewise cubic Bezier with bounded maximum curvature.
|
static int |
_BEZIER_SLACK
The defining type represents a G1-continuous, piecewise cubic Bezier with pseudo gravity slack.
|
static int |
_INTERPOLATION
The defining type represents a C1-continuous, interpolation spline.
|
static int |
_PARAMETRIC
The defining type represents a G1-continuous, parametric curve.
|
static int |
_UNSUPPORTED
The defining type is unsupported.
|
static SplinePathBuilder.DefiningTypes |
BEZIER
The defining type represents a G1-continuous, piecewise cubic Bezier.
|
static SplinePathBuilder.DefiningTypes |
BEZIER_MAX_CURVATURE
The defining type represents a G1-continuous, piecewise cubic Bezier with bounded maximum curvature.
|
static SplinePathBuilder.DefiningTypes |
BEZIER_SLACK
The defining type represents a G1-continuous, piecewise cubic Bezier with pseudo gravity slack.
|
static SplinePathBuilder.DefiningTypes |
INTERPOLATION
The defining type represents a C1-continuous, interpolation spline.
|
static SplinePathBuilder.DefiningTypes |
PARAMETRIC
The defining type represents a G1-continuous, parametric curve.
|
static SplinePathBuilder.DefiningTypes |
UNSUPPORTED
The defining type is unsupported.
|
Modifier and Type | Method and Description |
---|---|
static SplinePathBuilder.DefiningTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.DefiningTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.DefiningTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplinePathBuilder.DefiningTypes UNSUPPORTED
public static final SplinePathBuilder.DefiningTypes INTERPOLATION
public static final SplinePathBuilder.DefiningTypes PARAMETRIC
public static final SplinePathBuilder.DefiningTypes BEZIER
public static final SplinePathBuilder.DefiningTypes BEZIER_SLACK
public static final SplinePathBuilder.DefiningTypes BEZIER_MAX_CURVATURE
public static final int _UNSUPPORTED
public static final int _INTERPOLATION
public static final int _PARAMETRIC
public static final int _BEZIER
public static final int _BEZIER_SLACK
public static final int _BEZIER_MAX_CURVATURE
public static SplinePathBuilder.DefiningTypes valueOf(int value)
public static SplinePathBuilder.DefiningTypes valueOf(String name)
public static SplinePathBuilder.DefiningTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.