Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.BLOCK_UNIFY
Retain reason is because of the presence of the NX_BLOCK_UNIFY attribute
|
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.EQUIPMENT
Retain reason is the object is equipment and is not supported
|
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.EXPLICIT
Retain reason is the user explicitly marked it retain
|
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.NON_CLASSIFICATION
Retain reason is the object did not originate from classification and is not supported
|
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.UNSPECIFIED
Retain reason is not specified
|
Modifier and Type | Method and Description |
---|---|
RoutingBulkReplacementBuilderRetainReasonType |
BulkReplacementBuilder.getRetainReasonForObject(NXObject objectTag)
The retain reason getter
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingBulkReplacementBuilderRetainReasonType |
RoutingBulkReplacementBuilderRetainReasonType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingBulkReplacementBuilderRetainReasonType[] |
RoutingBulkReplacementBuilderRetainReasonType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.